<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic windows usb device disconnect reconnect  in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/windows-usb-device-disconnect-reconnect/m-p/782225#M47649</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a Kinetis Freedom K22F evaluation board. I have a program running that enables a USB CDC VCOM device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Windows sees the device just fine and communication is not a problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem I am having is each time I restart the debug session (I am using Segger J-Trace), I have to physically unplug and replug the USB CDC VCOM cable so I can talk to the device again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;either PuTTY and RealTerm to communicate with the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there some 'reset' register or reset sequence available with the K22F eval board that one can use to 'simulate' the disconnect and reconnection of the USB device?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Oct 2018 16:20:56 GMT</pubDate>
    <dc:creator>Keith4DSmith</dc:creator>
    <dc:date>2018-10-11T16:20:56Z</dc:date>
    <item>
      <title>windows usb device disconnect reconnect</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/windows-usb-device-disconnect-reconnect/m-p/782225#M47649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a Kinetis Freedom K22F evaluation board. I have a program running that enables a USB CDC VCOM device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Windows sees the device just fine and communication is not a problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem I am having is each time I restart the debug session (I am using Segger J-Trace), I have to physically unplug and replug the USB CDC VCOM cable so I can talk to the device again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;either PuTTY and RealTerm to communicate with the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there some 'reset' register or reset sequence available with the K22F eval board that one can use to 'simulate' the disconnect and reconnection of the USB device?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Oct 2018 16:20:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/windows-usb-device-disconnect-reconnect/m-p/782225#M47649</guid>
      <dc:creator>Keith4DSmith</dc:creator>
      <dc:date>2018-10-11T16:20:56Z</dc:date>
    </item>
    <item>
      <title>Re: windows usb device disconnect reconnect</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/windows-usb-device-disconnect-reconnect/m-p/782226#M47650</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Keith,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm making tests on my side to reproduce this behavior. Could you please tell me which version of Windows are you running?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Victor.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2018 15:41:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/windows-usb-device-disconnect-reconnect/m-p/782226#M47650</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-10-12T15:41:19Z</dc:date>
    </item>
    <item>
      <title>Re: windows usb device disconnect reconnect</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/windows-usb-device-disconnect-reconnect/m-p/782227#M47651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Windows 7 Enterprise Service Pack 1&lt;/P&gt;&lt;P&gt;Details of usbser.sys at attached in jpg&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74407iF602FF1E6393ECAE/image-size/large?v=v2&amp;amp;px=999" title="usbser.sys.jpg" alt="usbser.sys.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Oct 2018 16:00:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/windows-usb-device-disconnect-reconnect/m-p/782227#M47651</guid>
      <dc:creator>Keith4DSmith</dc:creator>
      <dc:date>2018-10-12T16:00:09Z</dc:date>
    </item>
    <item>
      <title>Re: windows usb device disconnect reconnect</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/windows-usb-device-disconnect-reconnect/m-p/782228#M47652</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Keith,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for providing more information. I was able to reproduce the behavior you mentioned using Windows7, the example dev_cdc_vcom_bm of the SDK v2.41 and Tera Term.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to the readme file about this behavior:&lt;/P&gt;&lt;P&gt;&amp;lt;MCUXpresso_SDK_Install&amp;gt;/boards/&amp;lt;board&amp;gt;/usb_examples/usb_device_cdc_vcom_lite/&amp;lt;rtos&amp;gt;/readme.pdf&lt;/P&gt;&lt;P&gt;Since there is no dynamic detection between host and device, the COM port must be closed from the terminal tool prior to plug-out/reset the CDC device. Or the CDC device won't get recognized next time you plug-in with the COM port still opened.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Oct 2018 19:26:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/windows-usb-device-disconnect-reconnect/m-p/782228#M47652</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-10-16T19:26:16Z</dc:date>
    </item>
  </channel>
</rss>