<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 SRAM_LOWER</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRAM-LOWER/m-p/781918#M47614</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can't seem to convince the linker to use the section SRAM_LOWER.&amp;nbsp; It overflows SRAM_UPPER without adding anything to the lower section.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Memory region Used Size Region Size %age Used&lt;BR /&gt; SRAM_UPPER: 262116 B 192 KB 133.32%&lt;BR /&gt; SRAM_LOWER: 0 GB 64 KB 0.00%&lt;BR /&gt;c:/nxp/mcuxpressoide_10.1.1_606/ide/tools/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/ld.exe: rtcpu16 Foundation.axf section `.bss' will not fit in region `SRAM_UPPER'&lt;BR /&gt; FLEX_RAM: 0 GB 4 KB 0.00%&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I utilize this memory?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Jun 2018 19:47:33 GMT</pubDate>
    <dc:creator>billmolleran</dc:creator>
    <dc:date>2018-06-14T19:47:33Z</dc:date>
    <item>
      <title>SRAM_LOWER</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRAM-LOWER/m-p/781918#M47614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can't seem to convince the linker to use the section SRAM_LOWER.&amp;nbsp; It overflows SRAM_UPPER without adding anything to the lower section.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Memory region Used Size Region Size %age Used&lt;BR /&gt; SRAM_UPPER: 262116 B 192 KB 133.32%&lt;BR /&gt; SRAM_LOWER: 0 GB 64 KB 0.00%&lt;BR /&gt;c:/nxp/mcuxpressoide_10.1.1_606/ide/tools/bin/../lib/gcc/arm-none-eabi/6.3.1/../../../../arm-none-eabi/bin/ld.exe: rtcpu16 Foundation.axf section `.bss' will not fit in region `SRAM_UPPER'&lt;BR /&gt; FLEX_RAM: 0 GB 4 KB 0.00%&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I utilize this memory?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jun 2018 19:47:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRAM-LOWER/m-p/781918#M47614</guid>
      <dc:creator>billmolleran</dc:creator>
      <dc:date>2018-06-14T19:47:33Z</dc:date>
    </item>
    <item>
      <title>Re: SRAM_LOWER</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRAM-LOWER/m-p/781919#M47615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi，&lt;/P&gt;&lt;P&gt;On the assumption that you are using MCUXpresso IDE, then please see chapter 14, "Memory Configuration and Linker Scripts", of the MCUXpresso IDE v10.1. User Guide for more details of how images are laid out in memory.&lt;/P&gt;&lt;P style="padding: 0px; min-height: 8pt;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There are various ways of moving the&amp;nbsp;heap, stack or&amp;nbsp;global variables into the second RAM bank described in this chapter - the simplest of which is probably to use the "memory configuration" editor, as shown in section 14.8 and 14.9.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jun 2018 02:04:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SRAM-LOWER/m-p/781919#M47615</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2018-06-15T02:04:51Z</dc:date>
    </item>
  </channel>
</rss>