<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCUXpresso and tailored FRDM-K64 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-and-tailored-FRDM-K64/m-p/781784#M47608</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Luis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will need an interface to program the K64-F. If you want to save pins I would recommend to use Serial Wire Debug (SWD) interface. Different from JTAG interface, SWD only takes two pins:&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;SWCLK = clock.&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;SWDIO = Data input/output.&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 21 Sep 2018 16:36:18 GMT</pubDate>
    <dc:creator>victorjimenez</dc:creator>
    <dc:date>2018-09-21T16:36:18Z</dc:date>
    <item>
      <title>MCUXpresso and tailored FRDM-K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-and-tailored-FRDM-K64/m-p/781783#M47607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am developing a networked solution based in FRDM-K64 board.&lt;/P&gt;&lt;P&gt;This board have a lot of nice features that I will not use and in the other hand I need to free some GPIOs to make use of them for this project .&lt;/P&gt;&lt;P&gt;So the idea is to design a tailored FRDM-K64 board without most of its periferal devices, the less components possible but keeping its ethernet capabilities.&lt;/P&gt;&lt;P&gt;One of the things that I need to get rid of, is the OpenSDA interface, If so... Is there anyway to make use of the the axf file generated by MCUXpresso? Haw can I program the MK64FN mcu without the OpenSDA interface?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Sep 2018 09:48:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-and-tailored-FRDM-K64/m-p/781783#M47607</guid>
      <dc:creator>luimarma</dc:creator>
      <dc:date>2018-09-20T09:48:08Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso and tailored FRDM-K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-and-tailored-FRDM-K64/m-p/781784#M47608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Luis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You will need an interface to program the K64-F. If you want to save pins I would recommend to use Serial Wire Debug (SWD) interface. Different from JTAG interface, SWD only takes two pins:&amp;nbsp;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;SWCLK = clock.&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;SWDIO = Data input/output.&amp;nbsp;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Sep 2018 16:36:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-and-tailored-FRDM-K64/m-p/781784#M47608</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-09-21T16:36:18Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso and tailored FRDM-K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-and-tailored-FRDM-K64/m-p/781785#M47609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Victor. This I have clear. Do you know if it is possible to setup MCU Expresso to program the board using the SWD interface?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Sep 2018 06:50:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-and-tailored-FRDM-K64/m-p/781785#M47609</guid>
      <dc:creator>luimarma</dc:creator>
      <dc:date>2018-09-24T06:50:06Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso and tailored FRDM-K64</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-and-tailored-FRDM-K64/m-p/781786#M47610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Luis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The fully featured debugger supports both SWD and JTAG debugging, and features direct download to on-chip and external flash memory.&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/MCUXpresso_IDE_User_Guide.pdf"&gt;Link to MCUXpresso IDE User Guide.&amp;nbsp;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;Victor.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 14:55:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCUXpresso-and-tailored-FRDM-K64/m-p/781786#M47610</guid>
      <dc:creator>victorjimenez</dc:creator>
      <dc:date>2018-09-25T14:55:39Z</dc:date>
    </item>
  </channel>
</rss>