<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Is it possible to run bluetooth demo applications with USB-KW41Z</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-it-possible-to-run-bluetooth-demo-applications-with-USB-KW41Z/m-p/780033#M47442</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;Bijesh C,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you can use the USB-KW41Z to run the Bluetooth demo applications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe you are using the&amp;nbsp;Kinetis KW41Z Connectivity Software (REV 1.0.2). This version of the software supports KDS and IAR IDEs. You can refer to the "&lt;EM&gt;&amp;lt;ConnSw&amp;gt;\docs\wireless\Bluetooth\&lt;STRONG&gt;BLE Quick Start Guide.pdf&lt;/STRONG&gt;&lt;/EM&gt;" document for instructions on how to run the demos.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that there is a newer version of the wireless stacks&amp;nbsp;available from the &lt;A _jive_internal="true" href="https://community.nxp.com/thread/I recommend using the newer wireless SDK from the&amp;nbsp;MCUXpresso SDK Builder. This newer SDK is supported in MCUXpresso v10.0.2 and IAR IDEs."&gt;MCUXpresso SDK Builder&lt;/A&gt;. This newer SDK is supported in MCUXpresso v10.0.2 and IAR IDEs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Dec 2017 22:06:11 GMT</pubDate>
    <dc:creator>gerardo_rodriguez</dc:creator>
    <dc:date>2017-12-14T22:06:11Z</dc:date>
    <item>
      <title>Is it possible to run bluetooth demo applications with USB-KW41Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-it-possible-to-run-bluetooth-demo-applications-with-USB-KW41Z/m-p/780032#M47441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Hi,&lt;BR /&gt;I am trying to run a bluetooth low energy demo application using USB-KW41Z device using the demo applications available with USB-KW41Z installation. But as per the&amp;nbsp;Bluetooth® Low Energy Demo Applications User’s Guide, the USB-KW41Z board is mainly targeted for sniffer applications and the demo application testing is done with&amp;nbsp;FRDM-KW41Z platform and a Bluetooth Low Energy capable central device. If the USB-KW41Z is not meant for bluetooth demo applications, what is the use of .launch files in FreeRTOS--&amp;gt;kds folder? And if USB-KW41Z can be used for bluetooth demo applications what is the procedure to be followed?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Regards,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Bijesh&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Nov 2017 05:56:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-it-possible-to-run-bluetooth-demo-applications-with-USB-KW41Z/m-p/780032#M47441</guid>
      <dc:creator>bijeshc</dc:creator>
      <dc:date>2017-11-16T05:56:37Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to run bluetooth demo applications with USB-KW41Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-it-possible-to-run-bluetooth-demo-applications-with-USB-KW41Z/m-p/780033#M47442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;Bijesh C,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you can use the USB-KW41Z to run the Bluetooth demo applications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe you are using the&amp;nbsp;Kinetis KW41Z Connectivity Software (REV 1.0.2). This version of the software supports KDS and IAR IDEs. You can refer to the "&lt;EM&gt;&amp;lt;ConnSw&amp;gt;\docs\wireless\Bluetooth\&lt;STRONG&gt;BLE Quick Start Guide.pdf&lt;/STRONG&gt;&lt;/EM&gt;" document for instructions on how to run the demos.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that there is a newer version of the wireless stacks&amp;nbsp;available from the &lt;A _jive_internal="true" href="https://community.nxp.com/thread/I recommend using the newer wireless SDK from the&amp;nbsp;MCUXpresso SDK Builder. This newer SDK is supported in MCUXpresso v10.0.2 and IAR IDEs."&gt;MCUXpresso SDK Builder&lt;/A&gt;. This newer SDK is supported in MCUXpresso v10.0.2 and IAR IDEs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Dec 2017 22:06:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-it-possible-to-run-bluetooth-demo-applications-with-USB-KW41Z/m-p/780033#M47442</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2017-12-14T22:06:11Z</dc:date>
    </item>
  </channel>
</rss>