<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: A problem for IAR When download the code to the K60F flash</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-problem-for-IAR-When-download-the-code-to-the-K60F-flash/m-p/228575#M4743</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That is probably a question for IAR.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Mar 2013 16:52:31 GMT</pubDate>
    <dc:creator>JimDon</dc:creator>
    <dc:date>2013-03-20T16:52:31Z</dc:date>
    <item>
      <title>A problem for IAR When download the code to the K60F flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-problem-for-IAR-When-download-the-code-to-the-K60F-flash/m-p/228573#M4741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I find a problem when I use IAR to download the code to the K60F flash.The IAR error report:"load the K60 flash reported error".At first I think it is fault with my circuit of processor,and I test two mode processor that are MK60FN1M and MK60FX512,but It has the same result.&lt;/P&gt;&lt;P&gt;My version of IAR is 6.4,and the I use two Debugger to test it that are J-link and OSBDM, I update the newest verion of OSBDM.When I use OSBDM,It can downloader the code with the icf file is 128K_Ram,but It doesn't work and report error with the icf file is 1M Pflash or 512KPflash.When I use J-link tool to connect the processor it,it reported "con't find any flash".&lt;/P&gt;&lt;P&gt;My MK60F circuit is as same as MK60D seriers and the MK60D can work,and the test code is TWR-MK60-120M.There are someting I don't pay attention?is that I need to test it use code warrior?please give me a help , Thank you very much!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Mar 2013 02:47:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-problem-for-IAR-When-download-the-code-to-the-K60F-flash/m-p/228573#M4741</guid>
      <dc:creator>AaronsCook</dc:creator>
      <dc:date>2013-03-18T02:47:56Z</dc:date>
    </item>
    <item>
      <title>Re: A problem for IAR When download the code to the K60F flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-problem-for-IAR-When-download-the-code-to-the-K60F-flash/m-p/228574#M4742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have solved this problem.In IAR 6.40,it must choose the MK70xxx128KB int the Debugger file that can&amp;nbsp; downloader the flash.but I use the MK60F why need to choose MK70's flash file?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2013 14:14:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-problem-for-IAR-When-download-the-code-to-the-K60F-flash/m-p/228574#M4742</guid>
      <dc:creator>AaronsCook</dc:creator>
      <dc:date>2013-03-20T14:14:48Z</dc:date>
    </item>
    <item>
      <title>Re: A problem for IAR When download the code to the K60F flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-problem-for-IAR-When-download-the-code-to-the-K60F-flash/m-p/228575#M4743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That is probably a question for IAR.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2013 16:52:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-problem-for-IAR-When-download-the-code-to-the-K60F-flash/m-p/228575#M4743</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2013-03-20T16:52:31Z</dc:date>
    </item>
    <item>
      <title>Re: A problem for IAR When download the code to the K60F flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-problem-for-IAR-When-download-the-code-to-the-K60F-flash/m-p/228576#M4744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regarding J-Link:&lt;/P&gt;&lt;P&gt;Sounds a bit like a problem in the IAR EWARM flashloader... We are not aware of any problems in the current J-Link software version.&lt;/P&gt;&lt;P&gt;Could you please do the following?:&lt;/P&gt;&lt;P&gt;- Download &amp;amp; install the latest J-Link software package (&lt;A href="http://www.segger.com/jlink-software.html"&gt;http://www.segger.com/jlink-software.html&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;- Update the DLL in the IAR directory via the DLLUpdater which is started automatically after the installation&lt;/P&gt;&lt;P&gt;- Use the J-Link flashloader instead of the EWARM flashloader. For more information about how to to this:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.segger.com/admin/uploads/productDocs/UM08001_JLinkARM.pdf" title="http://www.segger.com/admin/uploads/productDocs/UM08001_JLinkARM.pdf"&gt;http://www.segger.com/admin/uploads/productDocs/UM08001_JLinkARM.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Chapter "flash download", 6.4.1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Alex&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2013 13:28:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-problem-for-IAR-When-download-the-code-to-the-K60F-flash/m-p/228576#M4744</guid>
      <dc:creator>seggermicrocont</dc:creator>
      <dc:date>2013-03-21T13:28:26Z</dc:date>
    </item>
    <item>
      <title>Re: A problem for IAR When download the code to the K60F flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-problem-for-IAR-When-download-the-code-to-the-K60F-flash/m-p/228577#M4745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;thank you! I have test the processor with the J-Link.that's good! there is no problem with the current version.:smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;laplenden&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Mar 2013 06:58:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/A-problem-for-IAR-When-download-the-code-to-the-K60F-flash/m-p/228577#M4745</guid>
      <dc:creator>AaronsCook</dc:creator>
      <dc:date>2013-03-22T06:58:57Z</dc:date>
    </item>
  </channel>
</rss>