<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: K22: Not supported ADC Channel DP0 and DP1? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-supported-ADC-Channel-DP0-and-DP1/m-p/779446#M47413</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Thomas,&lt;/P&gt;&lt;P&gt;- It seems its a bug when using the ADC1_DP0 and ADC1_DP1 channel,&lt;/P&gt;&lt;P&gt;while I think Processor Expert IDE will be fixed , as to there will no update for this tool,&lt;/P&gt;&lt;P&gt;now we recommend use MCUXpresso Config Tools. &lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-config-tools:MCUXpresso-Config-Tools?fsrch=1&amp;amp;sr=2&amp;amp;pageNum=1" title="https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-config-tools:MCUXpresso-Config-Tools?fsrch=1&amp;amp;sr=2&amp;amp;pageNum=1"&gt;MCUXpresso Config Tools|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And I checked with KDS and CW with Processor Expert, there isn't this bug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- About the other channels ADC1_SE4b, ADC1_SE5b and ADC1_SE6b, please first refer&lt;/P&gt;&lt;P&gt;to the Typical Usage demo to check whether it can work well :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/7028i00CA3EEF680EE355/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Jan 2018 07:54:09 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2018-01-15T07:54:09Z</dc:date>
    <item>
      <title>K22: Not supported ADC Channel DP0 and DP1?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-supported-ADC-Channel-DP0-and-DP1/m-p/779443#M47410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using processor MK22FX512CMX12 and&amp;nbsp;I try to configure a High-Level ADC compoment for ADC1&amp;nbsp;and want to use&amp;nbsp;ADC1_DP0 and ADC1_DP1 as input pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I get the message from the underlaying ADC_LDD component:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Peripheral "ADC1_DP0/ADC0_DP3" does not support required hardware interface (A/D channel (pin))&amp;nbsp;Cob_Control&amp;nbsp;&amp;nbsp;AD2/A/D channel (pin)&amp;nbsp;Processor Expert Problem&lt;/LI&gt;&lt;LI&gt;Peripheral "ADC1_DP1" does not support required hardware interface (A/D channel (pin))&amp;nbsp;Cob_Control&amp;nbsp;&amp;nbsp;AD2/A/D channel (pin)&amp;nbsp;Processor Expert Problem&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This error also comes up if the only component I have in my project is an ADC_LDD for ADC1. I can't figure out why these both&amp;nbsp;pins are not allowed for usage. Can anybody help me please?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/87i1716AFB94B3E02CE/image-size/large?v=v2&amp;amp;px=999" title="ADC1_Channel0_NotSupported.jpg" alt="ADC1_Channel0_NotSupported.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jan 2018 18:12:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-supported-ADC-Channel-DP0-and-DP1/m-p/779443#M47410</guid>
      <dc:creator>thomas_k1</dc:creator>
      <dc:date>2018-01-10T18:12:49Z</dc:date>
    </item>
    <item>
      <title>Re: K22: Not supported ADC Channel DP0 and DP1?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-supported-ADC-Channel-DP0-and-DP1/m-p/779444#M47411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-userid="296842" data-username="thomas_k" href="https://community.nxp.com/people/thomas_k"&gt;Thomas &lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was wondering your chip number is MK22FX512CMX12 ?&lt;/P&gt;&lt;P&gt;Which IDE do you used ?&lt;/P&gt;&lt;P&gt;It's better if you provide the project, I need reproduce the problem first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jan 2018 02:48:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-supported-ADC-Channel-DP0-and-DP1/m-p/779444#M47411</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-01-11T02:48:41Z</dc:date>
    </item>
    <item>
      <title>Re: K22: Not supported ADC Channel DP0 and DP1?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-supported-ADC-Channel-DP0-and-DP1/m-p/779445#M47412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for your your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU is typo: correct is &lt;STRONG&gt;MK22FX512VMC12 in MAPBGA 121-pin package&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3614i7A500F6264A9713B/image-size/large?v=v2&amp;amp;px=999" title="MK22.jpg" alt="MK22.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Processor Expert Software 10.4&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3376i655510EAAAF7459F/image-size/large?v=v2&amp;amp;px=999" title="PE10.4.jpg" alt="PE10.4.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For building and debugging I work with iSystems winIDEA Software, though I think this is not important here.&lt;/P&gt;&lt;P&gt;Attached is the project so far. I just added to ADC1 the ADC1_DP1 channel which creates the error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In general it seems that I have problems using ADC1. As you can see I also try to use ADC1_SE4b, ADC1_SE5b and ADC1_SE6b. All of these can be configured, but they don't work. Changing inputs doesn't have any effect.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2018 08:10:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-supported-ADC-Channel-DP0-and-DP1/m-p/779445#M47412</guid>
      <dc:creator>thomas_k1</dc:creator>
      <dc:date>2018-01-12T08:10:43Z</dc:date>
    </item>
    <item>
      <title>Re: K22: Not supported ADC Channel DP0 and DP1?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-supported-ADC-Channel-DP0-and-DP1/m-p/779446#M47413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Thomas,&lt;/P&gt;&lt;P&gt;- It seems its a bug when using the ADC1_DP0 and ADC1_DP1 channel,&lt;/P&gt;&lt;P&gt;while I think Processor Expert IDE will be fixed , as to there will no update for this tool,&lt;/P&gt;&lt;P&gt;now we recommend use MCUXpresso Config Tools. &lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-config-tools:MCUXpresso-Config-Tools?fsrch=1&amp;amp;sr=2&amp;amp;pageNum=1" title="https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-config-tools:MCUXpresso-Config-Tools?fsrch=1&amp;amp;sr=2&amp;amp;pageNum=1"&gt;MCUXpresso Config Tools|NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And I checked with KDS and CW with Processor Expert, there isn't this bug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- About the other channels ADC1_SE4b, ADC1_SE5b and ADC1_SE6b, please first refer&lt;/P&gt;&lt;P&gt;to the Typical Usage demo to check whether it can work well :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/7028i00CA3EEF680EE355/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jan 2018 07:54:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-supported-ADC-Channel-DP0-and-DP1/m-p/779446#M47413</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-01-15T07:54:09Z</dc:date>
    </item>
    <item>
      <title>Re: K22: Not supported ADC Channel DP0 and DP1?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-supported-ADC-Channel-DP0-and-DP1/m-p/779447#M47414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alice,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for that info.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Changing the IDE is at this moment the same for me as doing it on registers directly. I will check this if I have some more time for the details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the 2nd part: Me feeling is that there a differences between ADC1_SE8 and ADC1_SE4b.The same signal connected to both pins work only for ADC1_SE8.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This maybe comes from this channel "ADC1_SE4a" vs "ADC1_4b". I currently try to find out whether or not I have to make a specific configuration to these channels.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edit: I can confirm that this issue depends on MUXSEL in ADC1_CFG2. This bit is not set correct by generated code from PE. Setting it manually makes the channels work as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again&lt;/P&gt;&lt;P&gt;Thomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2018 09:53:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-Not-supported-ADC-Channel-DP0-and-DP1/m-p/779447#M47414</guid>
      <dc:creator>thomas_k1</dc:creator>
      <dc:date>2018-01-30T09:53:51Z</dc:date>
    </item>
  </channel>
</rss>