<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Using Flexbus with K10 with 100 pin package</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Flexbus-with-K10-with-100-pin-package/m-p/228537#M4739</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The schematics looks fine, was PTB19 initiliazed to another mux function in your code? You may add some code snippet&amp;nbsp; for read operation immediately after the code of flexbus initialization, and check if FB_OE works well as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Jan 2014 02:40:25 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2014-01-14T02:40:25Z</dc:date>
    <item>
      <title>Using Flexbus with K10 with 100 pin package</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Flexbus-with-K10-with-100-pin-package/m-p/228534#M4736</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone.&amp;nbsp; The 100 pin package does not have all 32 pins of the buss on the Flexbus.&amp;nbsp; I have a project with 8megs of external ram connected to the flex bus.&amp;nbsp; The RAM chip has a 16 bit bus and I have a 16 bit latch on the lower 16 bits of the Flexbus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I can tell, the signals look OK for a write, but when I try to read, I get the latch signal, R/W signal, and CE signal, but not the OE signal.&amp;nbsp; It always stays high.&amp;nbsp; As far as I can tell, it was enabled by processor expert when I look at the PE code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried changing the OE pin to a generic IO pin and I am able to toggle the pin in software, so the pin is not shorted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anybody have any suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jan 2014 16:29:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Flexbus-with-K10-with-100-pin-package/m-p/228534#M4736</guid>
      <dc:creator>dporada</dc:creator>
      <dc:date>2014-01-10T16:29:40Z</dc:date>
    </item>
    <item>
      <title>Re: Using Flexbus with K10 with 100 pin package</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Flexbus-with-K10-with-100-pin-package/m-p/228535#M4737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Would you please show a snapshot of the connection between the external RAM and K10? and what is the part number for K10 that you are using?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your patience!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2014 08:38:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Flexbus-with-K10-with-100-pin-package/m-p/228535#M4737</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-01-13T08:38:52Z</dc:date>
    </item>
    <item>
      <title>Re: Using Flexbus with K10 with 100 pin package</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Flexbus-with-K10-with-100-pin-package/m-p/228536#M4738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here's a partial schematic.&amp;nbsp; The chip is a &lt;SPAN style="font-family: Times; font-size: 6pt; line-height: 1.5em;"&gt;MK10DN512VLL10.&amp;nbsp; There is an error in the schematic.&amp;nbsp; Pin 82 of the CPU should be connected to FB_AD5.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Times; font-size: 6pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="page" title="Page 1"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/41393i4E13A73F13772803/image-size/large?v=v2&amp;amp;px=999" title="Screen Shot 2014-01-13 at Mon, Jan 13, 2014   9.08.50 AM.png" alt="Screen Shot 2014-01-13 at Mon, Jan 13, 2014   9.08.50 AM.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2014 14:10:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Flexbus-with-K10-with-100-pin-package/m-p/228536#M4738</guid>
      <dc:creator>dporada</dc:creator>
      <dc:date>2014-01-13T14:10:21Z</dc:date>
    </item>
    <item>
      <title>Re: Using Flexbus with K10 with 100 pin package</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Flexbus-with-K10-with-100-pin-package/m-p/228537#M4739</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The schematics looks fine, was PTB19 initiliazed to another mux function in your code? You may add some code snippet&amp;nbsp; for read operation immediately after the code of flexbus initialization, and check if FB_OE works well as expected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;B.R&lt;/P&gt;&lt;P&gt;Kan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jan 2014 02:40:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Flexbus-with-K10-with-100-pin-package/m-p/228537#M4739</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-01-14T02:40:25Z</dc:date>
    </item>
    <item>
      <title>Re: Using Flexbus with K10 with 100 pin package</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Flexbus-with-K10-with-100-pin-package/m-p/228538#M4740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't know what caused the problem, but creating a new project seemed to work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jan 2014 14:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-Flexbus-with-K10-with-100-pin-package/m-p/228538#M4740</guid>
      <dc:creator>dporada</dc:creator>
      <dc:date>2014-01-27T14:23:34Z</dc:date>
    </item>
  </channel>
</rss>