<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックIs there an example available for creating a motor control application with Kinetis Motor Suite that is not using the Motion Planner?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-an-example-available-for-creating-a-motor-control/m-p/778610#M47365</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have used KMS to identify my motor parameters and create a simple motion plan using the USER_RUN_PLAN command that I successfully downloaded and ran on my eval platform.&amp;nbsp; I now would like to create an application using the USER_RUN_SPEED command and cannot get the motor to turn.&amp;nbsp; Is there an example of creating a project for applications other than running a motion plan?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Feb 2018 16:42:16 GMT</pubDate>
    <dc:creator>randyfields</dc:creator>
    <dc:date>2018-02-01T16:42:16Z</dc:date>
    <item>
      <title>Is there an example available for creating a motor control application with Kinetis Motor Suite that is not using the Motion Planner?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-an-example-available-for-creating-a-motor-control/m-p/778610#M47365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have used KMS to identify my motor parameters and create a simple motion plan using the USER_RUN_PLAN command that I successfully downloaded and ran on my eval platform.&amp;nbsp; I now would like to create an application using the USER_RUN_SPEED command and cannot get the motor to turn.&amp;nbsp; Is there an example of creating a project for applications other than running a motion plan?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Feb 2018 16:42:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-an-example-available-for-creating-a-motor-control/m-p/778610#M47365</guid>
      <dc:creator>randyfields</dc:creator>
      <dc:date>2018-02-01T16:42:16Z</dc:date>
    </item>
    <item>
      <title>Re: Is there an example available for creating a motor control application with Kinetis Motor Suite that is not using the Motion Planner?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-an-example-available-for-creating-a-motor-control/m-p/778611#M47366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Randy,&lt;/P&gt;&lt;P&gt;I appologize for the delay.&lt;/P&gt;&lt;P&gt;Pls post your questions to the following KMS community:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/community/kinetis/kms"&gt;https://community.nxp.com/community/kinetis/kms&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The engineer in KMS team will give you better reply.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Mar 2018 07:59:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-there-an-example-available-for-creating-a-motor-control/m-p/778611#M47366</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-03-02T07:59:54Z</dc:date>
    </item>
  </channel>
</rss>