<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックWhat do I do with the Die attach pad?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-do-I-do-with-the-Die-attach-pad/m-p/778410#M47354</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys, Nooby question here, should be pretty straightforward. I'm building a teensy powered device of my own and am currently creating an eagle component for the MKL02Z32VFG4 bootloader chip. What on earth do I do with the Die attach pad on the bottom? I'm guessing I want to connect it to to the board to disperse heat but should it be connected to ground or am I wrong entirely? Many thanks, Giga.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jun 2018 13:42:11 GMT</pubDate>
    <dc:creator>gigatech</dc:creator>
    <dc:date>2018-06-13T13:42:11Z</dc:date>
    <item>
      <title>What do I do with the Die attach pad?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-do-I-do-with-the-Die-attach-pad/m-p/778410#M47354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys, Nooby question here, should be pretty straightforward. I'm building a teensy powered device of my own and am currently creating an eagle component for the MKL02Z32VFG4 bootloader chip. What on earth do I do with the Die attach pad on the bottom? I'm guessing I want to connect it to to the board to disperse heat but should it be connected to ground or am I wrong entirely? Many thanks, Giga.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2018 13:42:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-do-I-do-with-the-Die-attach-pad/m-p/778410#M47354</guid>
      <dc:creator>gigatech</dc:creator>
      <dc:date>2018-06-13T13:42:11Z</dc:date>
    </item>
    <item>
      <title>Re: What do I do with the Die attach pad?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-do-I-do-with-the-Die-attach-pad/m-p/778411#M47355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The recommendation is connected to ground, please check&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN2467.pdf?fsrch=1&amp;amp;sr=9&amp;amp;pageNum=2"&gt;AN2467&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jun 2018 16:24:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-do-I-do-with-the-Die-attach-pad/m-p/778411#M47355</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2018-06-13T16:24:36Z</dc:date>
    </item>
  </channel>
</rss>