<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K8X SPI max speed (slave)</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K8X-SPI-max-speed-slave/m-p/776108#M47230</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;15M is the maximum operating frequency is measured with non-continuous CS and SCK. When DSPI is configured with continuous CS and SCK, there is a constraint that SPI clock should not be greater than 1/6 of bus clock, for example, when bus clock is 60MHz, SPI clock should not be greater than 10MHz. This is because of the bit sampling in slave mode need more than 1 clock.&lt;BR /&gt;I'm not sure if flexio work as SPI can fast than 30M. Please refer to this post:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/614738?et=watches.email.thread#614738"&gt;https://community.nxp.com/message/614738?et=watches.email.thread#614738&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Nov 2017 06:53:13 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2017-11-16T06:53:13Z</dc:date>
    <item>
      <title>K8X SPI max speed (slave)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K8X-SPI-max-speed-slave/m-p/776107#M47229</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SPI peripheral is clocked by bus clock (60 MHz), and is limited to bus clock/2 (30 MHz), according to the reference manual. However, the datasheet states that, when operating in slave mode, there is a limitation of 15 MHz to the module frequency. Why is that? Is this really the maximum speed that I can get from the SPI as slave? I need a transfer rate of ~30Mbps as a slave. Is there any serial interface available in the MCU that I can achieve this (using FlexIO, for example)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Nov 2017 03:15:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K8X-SPI-max-speed-slave/m-p/776107#M47229</guid>
      <dc:creator>felipeyamamoto</dc:creator>
      <dc:date>2017-11-15T03:15:24Z</dc:date>
    </item>
    <item>
      <title>Re: K8X SPI max speed (slave)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K8X-SPI-max-speed-slave/m-p/776108#M47230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;15M is the maximum operating frequency is measured with non-continuous CS and SCK. When DSPI is configured with continuous CS and SCK, there is a constraint that SPI clock should not be greater than 1/6 of bus clock, for example, when bus clock is 60MHz, SPI clock should not be greater than 10MHz. This is because of the bit sampling in slave mode need more than 1 clock.&lt;BR /&gt;I'm not sure if flexio work as SPI can fast than 30M. Please refer to this post:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/614738?et=watches.email.thread#614738"&gt;https://community.nxp.com/message/614738?et=watches.email.thread#614738&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Nov 2017 06:53:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K8X-SPI-max-speed-slave/m-p/776108#M47230</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2017-11-16T06:53:13Z</dc:date>
    </item>
  </channel>
</rss>