<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Kinetis USB Boot ROM - Now or Planned?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-USB-Boot-ROM-Now-or-Planned/m-p/228330#M4718</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I'm curious if Freescale has any plans to include a Boot ROM that supports the USB device mode on many of the parts in the kinetis portfolio.&amp;nbsp; Specifically, something akin to the EZ Port, but for USB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand there is code available that can be programmed into flash, but I am looking for a solution for a new part without resident code.&amp;nbsp; I do not see anything in the existing portfolio today.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Jan 2014 13:27:23 GMT</pubDate>
    <dc:creator>dvona</dc:creator>
    <dc:date>2014-01-10T13:27:23Z</dc:date>
    <item>
      <title>Kinetis USB Boot ROM - Now or Planned?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-USB-Boot-ROM-Now-or-Planned/m-p/228330#M4718</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I'm curious if Freescale has any plans to include a Boot ROM that supports the USB device mode on many of the parts in the kinetis portfolio.&amp;nbsp; Specifically, something akin to the EZ Port, but for USB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I understand there is code available that can be programmed into flash, but I am looking for a solution for a new part without resident code.&amp;nbsp; I do not see anything in the existing portfolio today.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-Dan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Jan 2014 13:27:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-USB-Boot-ROM-Now-or-Planned/m-p/228330#M4718</guid>
      <dc:creator>dvona</dc:creator>
      <dc:date>2014-01-10T13:27:23Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis USB Boot ROM - Now or Planned?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-USB-Boot-ROM-Now-or-Planned/m-p/228331#M4719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am afraid that option has not been announced yet, nor even as possibility.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Perla&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2014 21:28:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-USB-Boot-ROM-Now-or-Planned/m-p/228331#M4719</guid>
      <dc:creator>perlam_i_au</dc:creator>
      <dc:date>2014-02-18T21:28:37Z</dc:date>
    </item>
  </channel>
</rss>