<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: K24 input pin behavior</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K24-input-pin-behavior/m-p/774978#M47120</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Fred,&lt;/P&gt;&lt;P&gt;I have checked the internal ticket system, there are schmitt trigger circuit for each input cell. I have checked the&amp;nbsp; Input leakage current spec in data sheet of K24, it is 1uA, in other words, the impedance of input pin is 1M ohm.&lt;/P&gt;&lt;P&gt;I suppose that the quadrature module works if you remove the 120K ohm serial resistor, is it right?&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Dec 2017 05:38:19 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2017-12-13T05:38:19Z</dc:date>
    <item>
      <title>K24 input pin behavior</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K24-input-pin-behavior/m-p/774977#M47119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there an explanation for what I'm seeing on some MK24FN1M0VLL12 pins? The attached waveforms show an example, pin 98, which is PTB19. Channel 1 is a signal generator output and channel 2 is pin 98. The circuit essentially has a 121K resistor between the sig generator and pin 98.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mux0,jpg shows waveforms with the the PORTB_PCR19 MUX set to zero. There's a bit more than the 121K resistor in the circuit which accounts for the small attenuation you can see in both the high and low levels on channel 2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;mux6.jpg shows waveforms with PORTB_PCR19 MUX set to six, which is what's needed for the application. The 221K can't drive the input. I also set MUX to one with the same result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;offset6.jpg shows waveforms with some negative offset in the sig generator input. With very fine tweaking on the sig generator, waveform 2 can show some metastability. The only thing that maybe makes sense is the effect of a Schmitt trigger on the chip inputs, but the only reference I see&amp;nbsp; to Schmitt triggering in the ref manual or data sheet regards the RTC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So is the Schmitt guess correct or is there something else going on?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2017 00:54:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K24-input-pin-behavior/m-p/774977#M47119</guid>
      <dc:creator>fcw</dc:creator>
      <dc:date>2017-12-11T00:54:35Z</dc:date>
    </item>
    <item>
      <title>Re: K24 input pin behavior</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K24-input-pin-behavior/m-p/774978#M47120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Fred,&lt;/P&gt;&lt;P&gt;I have checked the internal ticket system, there are schmitt trigger circuit for each input cell. I have checked the&amp;nbsp; Input leakage current spec in data sheet of K24, it is 1uA, in other words, the impedance of input pin is 1M ohm.&lt;/P&gt;&lt;P&gt;I suppose that the quadrature module works if you remove the 120K ohm serial resistor, is it right?&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Dec 2017 05:38:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K24-input-pin-behavior/m-p/774978#M47120</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-12-13T05:38:19Z</dc:date>
    </item>
  </channel>
</rss>