<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FRM-KL26z USB host: ID pin connection in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRM-KL26z-USB-host-ID-pin-connection/m-p/774856#M47108</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to use FRDM-KL26 board as USB host. In the user guide (FRDMKL26ZUG), it says that&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Jumper J9 shall be connected to get power out of FRDM board in USB host mode&lt;/P&gt;&lt;P&gt;- Resister R8 shall be shorted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is, about shorting R8. I don't see that KL26 uC has a USB0_ID pin. In the&amp;nbsp;&lt;SPAN&gt;FRDM-KL26 board, I don't see that ID pin (TO_USB_ID_TP) is being connected to an USB_ID pin in uC. So, is this even required?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If I connect a USB memory stick on the other side, which will never act as USB host, cant i just manually set USB peripheral in USB host mode?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Nov 2017 09:29:17 GMT</pubDate>
    <dc:creator>tejainece</dc:creator>
    <dc:date>2017-11-14T09:29:17Z</dc:date>
    <item>
      <title>FRM-KL26z USB host: ID pin connection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRM-KL26z-USB-host-ID-pin-connection/m-p/774856#M47108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to use FRDM-KL26 board as USB host. In the user guide (FRDMKL26ZUG), it says that&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Jumper J9 shall be connected to get power out of FRDM board in USB host mode&lt;/P&gt;&lt;P&gt;- Resister R8 shall be shorted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is, about shorting R8. I don't see that KL26 uC has a USB0_ID pin. In the&amp;nbsp;&lt;SPAN&gt;FRDM-KL26 board, I don't see that ID pin (TO_USB_ID_TP) is being connected to an USB_ID pin in uC. So, is this even required?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;If I connect a USB memory stick on the other side, which will never act as USB host, cant i just manually set USB peripheral in USB host mode?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Nov 2017 09:29:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRM-KL26z-USB-host-ID-pin-connection/m-p/774856#M47108</guid>
      <dc:creator>tejainece</dc:creator>
      <dc:date>2017-11-14T09:29:17Z</dc:date>
    </item>
    <item>
      <title>Re: FRM-KL26z USB host: ID pin connection</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRM-KL26z-USB-host-ID-pin-connection/m-p/774857#M47109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ravi Reja Gudapati,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; When you want to use the FRDM-KL26 USB host, you need to connect ID pin to ground, actually, this pin is used to check the USB is host or the device.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; More details about the USB ID pin, you also can google it, the following information is for your reference:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67696i621E531E3310C360/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you connect a USB memory stick on the other side, which will never act as USB host,&amp;nbsp; that side ID pin need to float, but KL26 side, you still need to connect ID pin to Ground.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67795i93594D7D7BB43985/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Aug 2018 06:06:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRM-KL26z-USB-host-ID-pin-connection/m-p/774857#M47109</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-08-28T06:06:11Z</dc:date>
    </item>
  </channel>
</rss>