<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KM34 is always in reset after power ON. in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM34-is-always-in-reset-after-power-ON/m-p/774018#M47067</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arvind Reddy Maram,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Is this KM34 board designed by yourself? Have you downloaded the code to this chip before?&lt;/P&gt;&lt;P&gt;&amp;nbsp; To an empty KM34 chip, the reset pin have the sawtooth wave is correct, after the chip is flashed, the reset pin will be high.&lt;/P&gt;&lt;P&gt;&amp;nbsp; I think, you can use the JLINK associated with the JLINK command to check whether you can connect the ARM core or not?&lt;/P&gt;&lt;P&gt;&amp;nbsp; If you can't find the core, it means your board hardware have problems. RESET is low won't influence the flash download.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Feb 2018 03:31:32 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2018-02-27T03:31:32Z</dc:date>
    <item>
      <title>KM34 is always in reset after power ON.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM34-is-always-in-reset-after-power-ON/m-p/774017#M47066</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our KM34 device has the reset pin always low. The device seems to be keeping it low.&lt;/P&gt;&lt;P&gt;Due to this I am unable to program the device.&lt;/P&gt;&lt;P&gt;Any help or guidance is greatly appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Feb 2018 16:55:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM34-is-always-in-reset-after-power-ON/m-p/774017#M47066</guid>
      <dc:creator>armaram</dc:creator>
      <dc:date>2018-02-26T16:55:28Z</dc:date>
    </item>
    <item>
      <title>Re: KM34 is always in reset after power ON.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM34-is-always-in-reset-after-power-ON/m-p/774018#M47067</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arvind Reddy Maram,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Is this KM34 board designed by yourself? Have you downloaded the code to this chip before?&lt;/P&gt;&lt;P&gt;&amp;nbsp; To an empty KM34 chip, the reset pin have the sawtooth wave is correct, after the chip is flashed, the reset pin will be high.&lt;/P&gt;&lt;P&gt;&amp;nbsp; I think, you can use the JLINK associated with the JLINK command to check whether you can connect the ARM core or not?&lt;/P&gt;&lt;P&gt;&amp;nbsp; If you can't find the core, it means your board hardware have problems. RESET is low won't influence the flash download.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Feb 2018 03:31:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KM34-is-always-in-reset-after-power-ON/m-p/774018#M47067</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-02-27T03:31:32Z</dc:date>
    </item>
  </channel>
</rss>