<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: MKL13Z64 wakeup from VLPS by PIN</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL13Z64-wakeup-from-VLPS-by-PIN/m-p/773595#M47035</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jieqiu Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would highly recommend to add an external pull up in this pin, this could be triggering an interrupt that wake it up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Mar 2018 15:38:15 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2018-03-01T15:38:15Z</dc:date>
    <item>
      <title>MKL13Z64 wakeup from VLPS by PIN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL13Z64-wakeup-from-VLPS-by-PIN/m-p/773592#M47032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The device is programmed to go into the VLPS mode when the task is finished. It will be waken up by a button (gpio pin). It works fine and seems no any problem until I notice that occasionally the device in the VLPS mode can be randomly waken up without the button being touched.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Before the device is put into sleep, code disable most of the gpio pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas how I can deal with it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jan 2018 16:28:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL13Z64-wakeup-from-VLPS-by-PIN/m-p/773592#M47032</guid>
      <dc:creator>jqy</dc:creator>
      <dc:date>2018-01-31T16:28:34Z</dc:date>
    </item>
    <item>
      <title>Re: MKL13Z64 wakeup from VLPS by PIN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL13Z64-wakeup-from-VLPS-by-PIN/m-p/773593#M47033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jieqiu Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There could be many sources of interrupts that could wakeup the MCU as long as any interrupt could wakeup the MCU;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did the GPIO interrupt is the only one configured before your MCU goes to VLPS mode? I would recommend to isolate the issue by disabling all other possible interrupts and check if it is your GPIO interrupt or there is other source for the problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would also recommend to check the noise level in the pin that wakeup your MCU, if it is high, it could be the one that wake up your MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, the NMI interrupt could be being triggered, did you have an external pull up resistor in this pin?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information could help you.&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Feb 2018 00:38:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL13Z64-wakeup-from-VLPS-by-PIN/m-p/773593#M47033</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2018-02-03T00:38:05Z</dc:date>
    </item>
    <item>
      <title>Re: MKL13Z64 wakeup from VLPS by PIN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL13Z64-wakeup-from-VLPS-by-PIN/m-p/773594#M47034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Antonio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have two pins which can wake up the device.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The NMI pin is left unused. The pin has not been given an external pull up resistor. Is an internal pull up is good enough for it?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jieqiu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Feb 2018 10:22:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL13Z64-wakeup-from-VLPS-by-PIN/m-p/773594#M47034</guid>
      <dc:creator>jqy</dc:creator>
      <dc:date>2018-02-05T10:22:09Z</dc:date>
    </item>
    <item>
      <title>Re: MKL13Z64 wakeup from VLPS by PIN</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL13Z64-wakeup-from-VLPS-by-PIN/m-p/773595#M47035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jieqiu Yang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would highly recommend to add an external pull up in this pin, this could be triggering an interrupt that wake it up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Mar 2018 15:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL13Z64-wakeup-from-VLPS-by-PIN/m-p/773595#M47035</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2018-03-01T15:38:15Z</dc:date>
    </item>
  </channel>
</rss>