<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Linker Command File and Interrupt Vector Table in CW10.1 Project</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Linker-Command-File-and-Interrupt-Vector-Table-in-CW10-1-Project/m-p/157444#M470</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;were can I find and edit the Linker Command File in a K40 Project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have to find the ___VECTOR_RAM declaration. Because I get an error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Undefind:&amp;nbsp; ___VECTOR_RAM;&lt;/P&gt;&lt;P&gt;In my projekt ___VECTOR_RAM; is declared extern:&amp;nbsp;&lt;/P&gt;&lt;P&gt;extern uint_32 ___VECTOR_RAM[ ];﻿ &amp;nbsp; &amp;nbsp; &amp;nbsp; /* declared in P2.c */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Aug 2011 18:59:17 GMT</pubDate>
    <dc:creator>Thommi_Tulpe</dc:creator>
    <dc:date>2011-08-09T18:59:17Z</dc:date>
    <item>
      <title>Linker Command File and Interrupt Vector Table in CW10.1 Project</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Linker-Command-File-and-Interrupt-Vector-Table-in-CW10-1-Project/m-p/157444#M470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;were can I find and edit the Linker Command File in a K40 Project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have to find the ___VECTOR_RAM declaration. Because I get an error.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Undefind:&amp;nbsp; ___VECTOR_RAM;&lt;/P&gt;&lt;P&gt;In my projekt ___VECTOR_RAM; is declared extern:&amp;nbsp;&lt;/P&gt;&lt;P&gt;extern uint_32 ___VECTOR_RAM[ ];﻿ &amp;nbsp; &amp;nbsp; &amp;nbsp; /* declared in P2.c */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Aug 2011 18:59:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Linker-Command-File-and-Interrupt-Vector-Table-in-CW10-1-Project/m-p/157444#M470</guid>
      <dc:creator>Thommi_Tulpe</dc:creator>
      <dc:date>2011-08-09T18:59:17Z</dc:date>
    </item>
    <item>
      <title>Re: Linker Command File and Interrupt Vector Table in CW10.1 Project</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Linker-Command-File-and-Interrupt-Vector-Table-in-CW10-1-Project/m-p/157445#M471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Open the project settings and look in "C/C++ Build | Settings | ARM Linker | Input".&lt;/P&gt;&lt;P&gt;This will show you the "Linker Command File" with a path and the name of the *.lcf being used for the present target.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;By default this will be in a directory high up in the project hierarchy. By adding new location defines the exact location can be changed if required:&lt;/P&gt;&lt;P&gt;eg. "${APPLICATION_LOC}"/Project_Settings/Linker_Files/MK60N512VMD100_ram.lcf﻿&lt;/P&gt;&lt;P&gt;where the path variable APPLICATION_LOC is added as a path variable in the "Linked resources" register in the project properties.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2011 02:00:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Linker-Command-File-and-Interrupt-Vector-Table-in-CW10-1-Project/m-p/157445#M471</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2011-08-10T02:00:04Z</dc:date>
    </item>
    <item>
      <title>Re: Linker Command File and Interrupt Vector Table in CW10.1 Project</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Linker-Command-File-and-Interrupt-Vector-Table-in-CW10-1-Project/m-p/157446#M472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;thank you, this helps.&lt;/P&gt;&lt;P&gt;I also solved my problem with the&amp;nbsp; vector table.&lt;/P&gt;&lt;P&gt;In my project it has another name. I renamed it ant it works.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2011 15:04:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Linker-Command-File-and-Interrupt-Vector-Table-in-CW10-1-Project/m-p/157446#M472</guid>
      <dc:creator>Thommi_Tulpe</dc:creator>
      <dc:date>2011-08-10T15:04:55Z</dc:date>
    </item>
  </channel>
</rss>