<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Can't wake up from STOP with LPTMR</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-wake-up-from-STOP-with-LPTMR/m-p/769281#M46804</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which STOP mode is it that you are trying to use? Is it STOP or VLLS3?&lt;BR /&gt;Note that STOP (and VLPS etc.) are not low leakage modes and so won't be woken by the LLWU module since it is not operational in these.&lt;BR /&gt;LLS and VLLS modes &lt;SPAN style="text-decoration: underline;"&gt;will&lt;/SPAN&gt; be woken by the LLWU unit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This means that the 'standard' LPTMR interrupt will return you back to RUN mode from STOP modes and can wake from LLS modes via the wake up unit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Beware that these things can't really be tested with a debugger connected so always load and power cycle the board before doing tests to be sure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a attached a binary for the FRDM-K22F board so that you can get a feel for it. In the program I have configured a wake-up on SW2 (pressing it when in a LLS mode can wake up) and also on the LPTMR. The low power timer is clocked from the 32kHz RTC crystal (to match what I think you need) and it interrupts every 5s. When it interrupts it prints some text to inform from which power state it was interrupted in and toggles the RED LED- The green LED toggles faster (at 2.5Hz, driven from the SYSTICK instead).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Default is for the processor to be in WAIT mode but you can change this in the "Admin" menu on the VCOM interface at 115200 to check behavior in all K22 power modes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the command line interface where I show STOP, LLS3 and VLLS3 modes being entered, whereby the STOP mode will not retained after a LPTMR interrupt (to move back to WAIT mode hold SW3 down when the LPTMR message appears). You will see that the behavior in these modes is as theoretically expected:&lt;BR /&gt;- STOP mode freezes the SYSTICK operation but not the LPTMR&lt;BR /&gt;- LLS3 freezes SYSTICK but not LPTMR - LPTMR wakeup returns to RUN mode (and the handler sets itself to WAIT again). SW2 can also wake if pressed before the LPTMR interrupt arrives.&lt;BR /&gt;- VLLS3 is similar to LLS3 apart from the fact that it recovers via a reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;Hello&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; world&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; FRDM&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;K22F &lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;External&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;
Static memory &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x00000720&lt;/SPAN&gt;
OS Heap use &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x0219&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;0x6000&lt;/SPAN&gt;
Initial stack margin &lt;SPAN class="number token"&gt;0x0000978c&lt;/SPAN&gt;
WOKEN &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; restoring WAIT mode
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; initially the system is using WAIT mode
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT

Serial number&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;00&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt; enteer command line menu with ENTER key
Software version V1&lt;SPAN class="number token"&gt;.4&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;012&lt;/SPAN&gt;
Device identification&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; KINETIS

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Main menu
&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt;
&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Configure LAN interface
&lt;SPAN class="number token"&gt;2&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Configure serial interface
&lt;SPAN class="number token"&gt;3&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Go to I&lt;SPAN class="operator token"&gt;/&lt;/SPAN&gt;O menu
&lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Go to administration menu
&lt;SPAN class="number token"&gt;5&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Go to overview&lt;SPAN class="operator token"&gt;/&lt;/SPAN&gt;statistics menu
&lt;SPAN class="number token"&gt;6&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Go to USB menu
&lt;SPAN class="number token"&gt;7&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Go to I2C menu
&lt;SPAN class="number token"&gt;8&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Go to utFAT disk interface
&lt;SPAN class="number token"&gt;9&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTP&lt;SPAN class="operator token"&gt;/&lt;/SPAN&gt;TELNET commands
a&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN commands
help&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Display menu specific help
quit&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Leave command mode
&lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; move to Admin menu with &lt;SPAN class="number token"&gt;4&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;+&lt;/SPAN&gt; ENTER


&amp;nbsp;&amp;nbsp; Admin&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; menu
&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt;
up&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; go to main menu
show_config&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Show configuration
save&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Save configuration to FLASH
reject&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Reset non&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;saved changes
restore&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Restore factory settings
show_time&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Display date&lt;SPAN class="operator token"&gt;/&lt;/SPAN&gt;time
set_time&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Set time hh&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;mm&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;ss
set_date&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Set Date dd&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;mm&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;yyyy
show_alarm&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Display alarm d&lt;SPAN class="operator token"&gt;/&lt;/SPAN&gt;t
set_alarm&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Set alarm &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;date&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;+&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;time&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;
del_alarm&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Delete alarm
show_lp&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Show low power mode and options
set_lp&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;option&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; Set low power mode
reset&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Reset device
last_rst&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Reset cause
help&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Display menu specific help
quit&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Leave command mode
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
show_lp&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; show the power modes supported by the K22
&lt;SPAN class="number token"&gt;0&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; RUN
&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT &lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;active&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;
&lt;SPAN class="number token"&gt;2&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; STOP
&lt;SPAN class="number token"&gt;3&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; VLPR
&lt;SPAN class="number token"&gt;4&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; VLPW
&lt;SPAN class="number token"&gt;5&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; VLPS
&lt;SPAN class="number token"&gt;6&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; LLS2
&lt;SPAN class="number token"&gt;7&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; LLS3
&lt;SPAN class="number token"&gt;8&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; VLLS0
&lt;SPAN class="number token"&gt;9&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; VLLS1
&lt;SPAN class="number token"&gt;10&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; VLLS2
&lt;SPAN class="number token"&gt;11&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; VLLS3

&lt;SPAN class="property macro token"&gt;#LPTMR int. from 1 = WAIT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;---- LPTMR interrupt every 5s&lt;/SPAN&gt;
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
set_lp &lt;SPAN class="number token"&gt;2&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; command to move to STOP mode
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; now the green LED stips flashing and no UART entry is possible
&lt;SPAN class="property macro token"&gt;#LPTMR int. from 2 = STOP&lt;/SPAN&gt;
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;2&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; STOP&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; the LPTMT interrupt still works
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;2&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; STOP
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; here I have held SW3 so the interrupt sets back to WAIT mode
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
set_lp &lt;SPAN class="number token"&gt;7&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt; back in WAIT mode the UART works again and the green LED blinks

&lt;SPAN class="property macro token"&gt;#LPTMR int. from 6 = LLS2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;---- LLS2 is similar to STOP (no green LED)&lt;/SPAN&gt;
WOKEN &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; restoring WAIT mode&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt; after max 5s the LPTMR wakes and retuns the system to WAIT mode
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
set_lp &lt;SPAN class="number token"&gt;11&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; VLLS3 commaned here

&lt;SPAN class="property macro token"&gt;#

Hello, world... FRDM-K22F [Wakeup]&amp;nbsp; &amp;lt;--- afer max. 5s the LPTMR wakes via RESET (note reset cause)&lt;/SPAN&gt;
Static memory &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x00000720&lt;/SPAN&gt;
OS Heap use &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x0219&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;0x6000&lt;/SPAN&gt;
Initial stack margin &lt;SPAN class="number token"&gt;0x0000978c&lt;/SPAN&gt;
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
WOKEN &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; restoring WAIT mode
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have specific questions I can explain more details and show you operational code for whatever cases are required.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;SPAN&gt;Kinetis: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis.html" rel="nofollow noopener noreferrer" target="_blank"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Apr 2018 02:05:05 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2018-04-26T02:05:05Z</dc:date>
    <item>
      <title>Can't wake up from STOP with LPTMR</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-wake-up-from-STOP-with-LPTMR/m-p/769280#M46803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Processor: K22FN512 64-pin&lt;/P&gt;&lt;P&gt;Board:&amp;nbsp; Custom and FRDM-K22F&lt;/P&gt;&lt;P&gt;IDE:&amp;nbsp; KDS and Processor Expert&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/ErichS"&gt;ErichS&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problem is I am unable to wake from LPTMR when in STOP MODE.&lt;/P&gt;&lt;P&gt;It works fine if I use the function&lt;/P&gt;&lt;P&gt;Cpu_SetOperationMode(DOM_SLEEP, NULL, NULL);&lt;/P&gt;&lt;P&gt;or&lt;/P&gt;&lt;P&gt;Cpu_SetOperationMode(DOM_WAIT, NULL, NULL);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;with DOM_STOP, it never wakes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Clock source is 32KHz crystal (confirmed it always oscillates, even in stop)&lt;/P&gt;&lt;P&gt;Here are the settings for the CPU&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2786iE23387F54B15514B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have set up the LLWU as well, &lt;SPAN style="text-decoration: underline;"&gt;but the interrupt is never called &lt;/SPAN&gt;(even in SLEEP or WAIT)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2879iFD7AA11B5F32AF10/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This interrupt function gets called in DOM_SLEEP or DOM_WAIT after the LPTMR0 completes the count.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;PE_ISR(Wakeup_Timer)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;LPTMR_PDD_ClearInterruptFlag(LPTMR0_DEVICE);&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;And here is the main routine that blinks LED 10 times and goes to LP mode.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; for(;;){&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; /*&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp;* blink led 10 times&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp;*/&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; while(i&amp;lt;10){&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; HB_LED_ON;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; WAIT1_Waitms(200);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; HB_LED_OFF;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; WAIT1_Waitms(200);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; i++;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; }&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; i=0;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; /*&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp;&amp;nbsp; * go into low power mode&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; */&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; LPTMR0_CSR |= 1;&amp;nbsp; //enable timer&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; Cpu_SetOperationMode(DOM_STOP, NULL, NULL);//works if use DOM_WAIT or DOM_SLEEP&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;&amp;nbsp; LPTMR0_CSR &amp;amp;= ~1; //disable timer&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: courier\ new, courier, monospace;"&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2018 20:35:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-wake-up-from-STOP-with-LPTMR/m-p/769280#M46803</guid>
      <dc:creator>bcstewart</dc:creator>
      <dc:date>2018-04-25T20:35:01Z</dc:date>
    </item>
    <item>
      <title>Re: Can't wake up from STOP with LPTMR</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-wake-up-from-STOP-with-LPTMR/m-p/769281#M46804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which STOP mode is it that you are trying to use? Is it STOP or VLLS3?&lt;BR /&gt;Note that STOP (and VLPS etc.) are not low leakage modes and so won't be woken by the LLWU module since it is not operational in these.&lt;BR /&gt;LLS and VLLS modes &lt;SPAN style="text-decoration: underline;"&gt;will&lt;/SPAN&gt; be woken by the LLWU unit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This means that the 'standard' LPTMR interrupt will return you back to RUN mode from STOP modes and can wake from LLS modes via the wake up unit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Beware that these things can't really be tested with a debugger connected so always load and power cycle the board before doing tests to be sure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a attached a binary for the FRDM-K22F board so that you can get a feel for it. In the program I have configured a wake-up on SW2 (pressing it when in a LLS mode can wake up) and also on the LPTMR. The low power timer is clocked from the 32kHz RTC crystal (to match what I think you need) and it interrupts every 5s. When it interrupts it prints some text to inform from which power state it was interrupted in and toggles the RED LED- The green LED toggles faster (at 2.5Hz, driven from the SYSTICK instead).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Default is for the processor to be in WAIT mode but you can change this in the "Admin" menu on the VCOM interface at 115200 to check behavior in all K22 power modes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the command line interface where I show STOP, LLS3 and VLLS3 modes being entered, whereby the STOP mode will not retained after a LPTMR interrupt (to move back to WAIT mode hold SW3 down when the LPTMR message appears). You will see that the behavior in these modes is as theoretically expected:&lt;BR /&gt;- STOP mode freezes the SYSTICK operation but not the LPTMR&lt;BR /&gt;- LLS3 freezes SYSTICK but not LPTMR - LPTMR wakeup returns to RUN mode (and the handler sets itself to WAIT again). SW2 can also wake if pressed before the LPTMR interrupt arrives.&lt;BR /&gt;- VLLS3 is similar to LLS3 apart from the fact that it recovers via a reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;Hello&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; world&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; FRDM&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;K22F &lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;External&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;
Static memory &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x00000720&lt;/SPAN&gt;
OS Heap use &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x0219&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;0x6000&lt;/SPAN&gt;
Initial stack margin &lt;SPAN class="number token"&gt;0x0000978c&lt;/SPAN&gt;
WOKEN &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; restoring WAIT mode
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; initially the system is using WAIT mode
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT

Serial number&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;00&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt; enteer command line menu with ENTER key
Software version V1&lt;SPAN class="number token"&gt;.4&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;012&lt;/SPAN&gt;
Device identification&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt; KINETIS

&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Main menu
&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt;
&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Configure LAN interface
&lt;SPAN class="number token"&gt;2&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Configure serial interface
&lt;SPAN class="number token"&gt;3&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Go to I&lt;SPAN class="operator token"&gt;/&lt;/SPAN&gt;O menu
&lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Go to administration menu
&lt;SPAN class="number token"&gt;5&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Go to overview&lt;SPAN class="operator token"&gt;/&lt;/SPAN&gt;statistics menu
&lt;SPAN class="number token"&gt;6&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Go to USB menu
&lt;SPAN class="number token"&gt;7&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Go to I2C menu
&lt;SPAN class="number token"&gt;8&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Go to utFAT disk interface
&lt;SPAN class="number token"&gt;9&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FTP&lt;SPAN class="operator token"&gt;/&lt;/SPAN&gt;TELNET commands
a&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CAN commands
help&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Display menu specific help
quit&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Leave command mode
&lt;SPAN class="number token"&gt;4&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; move to Admin menu with &lt;SPAN class="number token"&gt;4&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;+&lt;/SPAN&gt; ENTER


&amp;nbsp;&amp;nbsp; Admin&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; menu
&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt;
up&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; go to main menu
show_config&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Show configuration
save&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Save configuration to FLASH
reject&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Reset non&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;saved changes
restore&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Restore factory settings
show_time&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Display date&lt;SPAN class="operator token"&gt;/&lt;/SPAN&gt;time
set_time&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Set time hh&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;mm&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;ss
set_date&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Set Date dd&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;mm&lt;SPAN class="punctuation token"&gt;:&lt;/SPAN&gt;yyyy
show_alarm&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Display alarm d&lt;SPAN class="operator token"&gt;/&lt;/SPAN&gt;t
set_alarm&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Set alarm &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;date&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;+&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;time&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;
del_alarm&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Delete alarm
show_lp&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Show low power mode and options
set_lp&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;option&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; Set low power mode
reset&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Reset device
last_rst&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Reset cause
help&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Display menu specific help
quit&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Leave command mode
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
show_lp&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; show the power modes supported by the K22
&lt;SPAN class="number token"&gt;0&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; RUN
&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT &lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;active&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt;
&lt;SPAN class="number token"&gt;2&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; STOP
&lt;SPAN class="number token"&gt;3&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; VLPR
&lt;SPAN class="number token"&gt;4&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; VLPW
&lt;SPAN class="number token"&gt;5&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; VLPS
&lt;SPAN class="number token"&gt;6&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; LLS2
&lt;SPAN class="number token"&gt;7&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; LLS3
&lt;SPAN class="number token"&gt;8&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; VLLS0
&lt;SPAN class="number token"&gt;9&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; VLLS1
&lt;SPAN class="number token"&gt;10&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; VLLS2
&lt;SPAN class="number token"&gt;11&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; VLLS3

&lt;SPAN class="property macro token"&gt;#LPTMR int. from 1 = WAIT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;---- LPTMR interrupt every 5s&lt;/SPAN&gt;
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
set_lp &lt;SPAN class="number token"&gt;2&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; command to move to STOP mode
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; now the green LED stips flashing and no UART entry is possible
&lt;SPAN class="property macro token"&gt;#LPTMR int. from 2 = STOP&lt;/SPAN&gt;
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;2&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; STOP&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; the LPTMT interrupt still works
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;2&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; STOP
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; here I have held SW3 so the interrupt sets back to WAIT mode
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
set_lp &lt;SPAN class="number token"&gt;7&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt; back in WAIT mode the UART works again and the green LED blinks

&lt;SPAN class="property macro token"&gt;#LPTMR int. from 6 = LLS2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;lt;---- LLS2 is similar to STOP (no green LED)&lt;/SPAN&gt;
WOKEN &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; restoring WAIT mode&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt; after max 5s the LPTMR wakes and retuns the system to WAIT mode
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
set_lp &lt;SPAN class="number token"&gt;11&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN class="operator token"&gt;&amp;lt;&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;--&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; VLLS3 commaned here

&lt;SPAN class="property macro token"&gt;#

Hello, world... FRDM-K22F [Wakeup]&amp;nbsp; &amp;lt;--- afer max. 5s the LPTMR wakes via RESET (note reset cause)&lt;/SPAN&gt;
Static memory &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x00000720&lt;/SPAN&gt;
OS Heap use &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x0219&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;0x6000&lt;/SPAN&gt;
Initial stack margin &lt;SPAN class="number token"&gt;0x0000978c&lt;/SPAN&gt;
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
WOKEN &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt; restoring WAIT mode
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT
LPTMR &lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt; from &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; WAIT&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have specific questions I can explain more details and show you operational code for whatever cases are required.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;SPAN&gt;Kinetis: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis.html" rel="nofollow noopener noreferrer" target="_blank"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Apr 2018 02:05:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-wake-up-from-STOP-with-LPTMR/m-p/769281#M46804</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-04-26T02:05:05Z</dc:date>
    </item>
    <item>
      <title>Re: Can't wake up from STOP with LPTMR</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-wake-up-from-STOP-with-LPTMR/m-p/769282#M46805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the binary.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My client is using Processor Expert (PE) and FreeRTOS. I would like to move them to bare-metal (BM) or even uTasker (which I've used in the past and prefer it over FreeRTOS).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to go to some low power stop mode, such as VLPS.&amp;nbsp; The few extra microamps is OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But for now, I need a PE/BM example.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Apr 2018 15:37:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-wake-up-from-STOP-with-LPTMR/m-p/769282#M46805</guid>
      <dc:creator>bcstewart</dc:creator>
      <dc:date>2018-04-26T15:37:34Z</dc:date>
    </item>
    <item>
      <title>Re: Can't wake up from STOP with LPTMR</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-wake-up-from-STOP-with-LPTMR/m-p/769283#M46806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;VLPS is not a LLWU mode so you simply need a working LPTMR interrupt.&lt;BR /&gt;Also, if the WAIT mode works you can simply set&lt;BR /&gt;SMC_PMCTRL = (SMC_PMCTRL_RUNM_NORMAL | SMC_PMCTRL_STOPM_VLPS | SMC_PMCTRL_LPWUI);&lt;BR /&gt;and &lt;BR /&gt;SYSTEM_CONTROL_REGISTER |= SLEEPDEEP;&lt;/P&gt;&lt;P&gt;manually before calling the WAIT mode to get the same result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know how good PE generated code is in this respect but if you are not saving power make sure that you add code to its startup (which may be missing) to set SMC_PMPROT_AVLP in SMC_PMPROT register to enable the VLPS mode. Beware that the register is a "write-once" register and you need to power cycle the system if it has been written before to allow different modes to be used.&lt;BR /&gt;Again, I can imaging that PE generated code may not be suitable for dynamically changing systems where more that one mode is used so you may need to generate code for each mode you want to test, load it, power cycle, test and repeat for each to be sure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that uTasker now incorporates FreeRTOS V9.0 for all devices so one can use uTasker OS, FreeRTOS OS or a mixture of both depending on which characteristics suit best. FreeRTOS and dynamic low power is however tricky. uTasker OS is optimised for dynamic low power operation which makes dynamic low power demos (and complete application) simple (as in binary file).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Good luck&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;P.S. PE generated code is simply copy-pasting some library code for you. If you have good library code that already does this (and works) I don't know that PE generated code has any real advantages. At the end of the day it is the reliable library code in operation that matters and not that it was configured in a GUI and generated.&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Apr 2018 16:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-wake-up-from-STOP-with-LPTMR/m-p/769283#M46806</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-04-26T16:18:30Z</dc:date>
    </item>
  </channel>
</rss>