<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: VLPS on Kinetis, Using TSS library for Touch input.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VLPS-on-Kinetis-Using-TSS-library-for-Touch-input/m-p/765852#M46597</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is not a link. You should goto &lt;A href="https://mcuxpresso.nxp.com/en/welcome"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt;&amp;nbsp;to download MK20 SDK package. The example is in that package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Jan 2018 09:23:35 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2018-01-30T09:23:35Z</dc:date>
    <item>
      <title>VLPS on Kinetis, Using TSS library for Touch input.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VLPS-on-Kinetis-Using-TSS-library-for-Touch-input/m-p/765849#M46594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;BR /&gt;Anybody here, using TSS library for touch input and configured the system for VLPS (Very Low Power Stop) mode for low power consumption?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm configuring my system to enter VLPS mode if no touch is detected for some time. After entering the low power mode, on Touch Input, the system isn't generating any kind of interrupt. I have tried manual configuration and with processor expert aswell without any success. The problem comes when I execute SLEEPDEEP command, and when processor enters into deepsleep. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS: I configured the system for LLS (Low Leakage Stop) mode, and everything worked fine, however, in LLS mode only one elctrode is active. Since my system's req. is that all the electrodes should be active in low power consumtion or in standy state.&lt;/P&gt;&lt;P&gt;Anybody else faced or facing the same issue in VLPS mode? I'm working on Kinetis K10 uC.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Please comment, I need some serious help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jan 2018 12:38:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/VLPS-on-Kinetis-Using-TSS-library-for-Touch-input/m-p/765849#M46594</guid>
      <dc:creator>taimurwajad123</dc:creator>
      <dc:date>2018-01-29T12:38:07Z</dc:date>
    </item>
    <item>
      <title>Re: VLPS on Kinetis, Using TSS library for Touch input.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VLPS-on-Kinetis-Using-TSS-library-for-Touch-input/m-p/765850#M46595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Taimur,&lt;/P&gt;&lt;P&gt;Please refer to SDK_2.2_MK20DX256xxx10.zip\boards\twrk60d100m\driver_examples\tsi_v2\low_power. I think this is a good exsample for you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2018 03:34:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/VLPS-on-Kinetis-Using-TSS-library-for-Touch-input/m-p/765850#M46595</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2018-01-30T03:34:22Z</dc:date>
    </item>
    <item>
      <title>Re: VLPS on Kinetis, Using TSS library for Touch input.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VLPS-on-Kinetis-Using-TSS-library-for-Touch-input/m-p/765851#M46596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jing,&lt;BR /&gt;Thanks for the reply. Unfortunately, can't open the link, can you please post the correct link?&lt;BR /&gt;&lt;BR /&gt;Thanks and Best Regards,&lt;BR /&gt;Taimur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2018 08:34:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/VLPS-on-Kinetis-Using-TSS-library-for-Touch-input/m-p/765851#M46596</guid>
      <dc:creator>taimurwajad123</dc:creator>
      <dc:date>2018-01-30T08:34:22Z</dc:date>
    </item>
    <item>
      <title>Re: VLPS on Kinetis, Using TSS library for Touch input.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/VLPS-on-Kinetis-Using-TSS-library-for-Touch-input/m-p/765852#M46597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;This is not a link. You should goto &lt;A href="https://mcuxpresso.nxp.com/en/welcome"&gt;https://mcuxpresso.nxp.com/en/welcome&lt;/A&gt;&amp;nbsp;to download MK20 SDK package. The example is in that package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2018 09:23:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/VLPS-on-Kinetis-Using-TSS-library-for-Touch-input/m-p/765852#M46597</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2018-01-30T09:23:35Z</dc:date>
    </item>
  </channel>
</rss>