<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKV46 GPIO PORTC4 setup as an output.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-GPIO-PORTC4-setup-as-an-output/m-p/765232#M46581</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am setting up a GPIO PortC4 as an output (to drive a /MR input on an ADM8322). I set the output high when I go through port setup and initialization. What I see with is scope is narrow low pulses on the output even though I am not toggling, or otherwise changing the state of the output. This causes reset to be triggered by the ADM8322, and keeps the MCU resetting. I there anyway to keep the low going pulses from occurring?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Brian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Apr 2018 16:26:18 GMT</pubDate>
    <dc:creator>bitjockey</dc:creator>
    <dc:date>2018-04-24T16:26:18Z</dc:date>
    <item>
      <title>KV46 GPIO PORTC4 setup as an output.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-GPIO-PORTC4-setup-as-an-output/m-p/765232#M46581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am setting up a GPIO PortC4 as an output (to drive a /MR input on an ADM8322). I set the output high when I go through port setup and initialization. What I see with is scope is narrow low pulses on the output even though I am not toggling, or otherwise changing the state of the output. This causes reset to be triggered by the ADM8322, and keeps the MCU resetting. I there anyway to keep the low going pulses from occurring?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Brian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Apr 2018 16:26:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-GPIO-PORTC4-setup-as-an-output/m-p/765232#M46581</guid>
      <dc:creator>bitjockey</dc:creator>
      <dc:date>2018-04-24T16:26:18Z</dc:date>
    </item>
    <item>
      <title>Re: KV46 GPIO PORTC4 setup as an output.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-GPIO-PORTC4-setup-as-an-output/m-p/765233#M46582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brian,&lt;/P&gt;&lt;P&gt;Sorry for the late reply!&lt;BR /&gt;For most digital pins, it keep the high impedance during reset phase, so you can add the external pull-up resistor to ensure it to be high level during reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 May 2018 07:55:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV46-GPIO-PORTC4-setup-as-an-output/m-p/765233#M46582</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2018-05-02T07:55:56Z</dc:date>
    </item>
  </channel>
</rss>