<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: LVD Module operation for Kinetis KE1xF Series Microcontroller</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LVD-Module-operation-for-Kinetis-KE1xF-Series-Microcontroller/m-p/764044#M46533</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000;"&gt;Hello,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000;"&gt;Well, I do not think that the manual spec has problems with LVD. Actually&amp;nbsp;&lt;SPAN class=""&gt;rising threshold is:&lt;BR /&gt;Rising threshold of LVR (Low Voltage Reset) = 2.7V + 45mV = 2.745V.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Apr 2018 08:52:29 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2018-04-25T08:52:29Z</dc:date>
    <item>
      <title>LVD Module operation for Kinetis KE1xF Series Microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LVD-Module-operation-for-Kinetis-KE1xF-Series-Microcontroller/m-p/764043#M46532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using the Kinetis series KE1xF Microcontroller in my application.&lt;/P&gt;&lt;P&gt;The power supply to the microcontroller is set at 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to know the LVD module functionality when the Power supply is set to 5V.&lt;/P&gt;&lt;P&gt;In the datasheet, the falling Low voltage detect threshold is mentioned as 2.88V. Attached is snapshot for the same.&lt;/P&gt;&lt;P&gt;but when the supply voltage to microcontroller is 5V, what is the Low voltage detect threshold in this case? I suppose it cannot be 2.88V as the microcontroller cannot operate below 4V in case the supply voltage is set to 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make me understand the LVD module operation and the corresponding reset scenarios&amp;nbsp;&amp;nbsp;in case the supply voltage is set to 5V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Kunmit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Apr 2018 11:36:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LVD-Module-operation-for-Kinetis-KE1xF-Series-Microcontroller/m-p/764043#M46532</guid>
      <dc:creator>kunmitpatra</dc:creator>
      <dc:date>2018-04-24T11:36:03Z</dc:date>
    </item>
    <item>
      <title>Re: LVD Module operation for Kinetis KE1xF Series Microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LVD-Module-operation-for-Kinetis-KE1xF-Series-Microcontroller/m-p/764044#M46533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000;"&gt;Hello,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000;"&gt;Well, I do not think that the manual spec has problems with LVD. Actually&amp;nbsp;&lt;SPAN class=""&gt;rising threshold is:&lt;BR /&gt;Rising threshold of LVR (Low Voltage Reset) = 2.7V + 45mV = 2.745V.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2018 08:52:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LVD-Module-operation-for-Kinetis-KE1xF-Series-Microcontroller/m-p/764044#M46533</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2018-04-25T08:52:29Z</dc:date>
    </item>
  </channel>
</rss>