<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Can't use OpenOCD with MKW24 Kinetis MCU</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-use-OpenOCD-with-MKW24-Kinetis-MCU/m-p/763354#M46492</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Matthieu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which flash programmer or IDE do you used ?&lt;/P&gt;&lt;P&gt;Have you select the right chip configuration when flash ?&lt;/P&gt;&lt;P&gt;And what about the debug interface inside OpenOCD， check it in the Device Manager :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2564iCB660114D7C5C491/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Dec 2017 09:53:42 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2017-12-07T09:53:42Z</dc:date>
    <item>
      <title>Can't use OpenOCD with MKW24 Kinetis MCU</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-use-OpenOCD-with-MKW24-Kinetis-MCU/m-p/763353#M46491</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everybody,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem using the MKW24 MCU with OpenOCD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I plug openocd and I use it, it seems to work properly (it discover the processor successfully):&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;Open On-Chip Debugger 0.10.0
Licensed under GNU GPL v2
For bug reports, read
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;http://openocd.org/doc/doxygen/bugs.html
Info : auto-selecting first available session transport "jtag". To override use 'transport select &amp;lt;transport&amp;gt;'.
Info : add flash_bank kinetis k22.flash
adapter speed: 1000 kHz
cortex_m reset_config sysresetreq
srst_only separate srst_nogate srst_open_drain connect_assert_srst
COM_PROGRAM_V7
Info : clock speed 1000 kHz
Info : JTAG tap: k22.cpu tap/device found: 0x4ba00477 (mfg: 0x23b (ARM Ltd.), part: 0xba00, ver: 0x4)
Info : k22.cpu: hardware has 6 breakpoints, 4 watchpoints
Info : MDM: Chip is unsecured. Continuing.
Info : accepting 'telnet' connection on tcp/4444
Initializing..
 INFO&amp;nbsp; Mass Erasing...
 INFO&amp;nbsp; Mass Erasing... Done
target halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0xfffffffe msp: 0xfffffffc
Info : JTAG tap: k22.cpu tap/device found: 0x4ba00477 (mfg: 0x23b (ARM Ltd.), part: 0xba00, ver: 0x4)
Info : MDM: Chip is unsecured. Continuing.
target halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0xfffffffe msp: 0xfffffffc
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when I try to flash it, I always get the following error message:&lt;/P&gt;&lt;PRE class="language-none line-numbers"&gt;&lt;CODE&gt;Arbitrary Flash Configuration Field writes enabled.
Protection info writes to FCF disabled.
Warn : BEWARE: incorrect flash configuration may permanently lock the device.
auto erase enabled
Error: Unsupported K-family FAMID
Error: MCU is unsupported, SDID 0x00009265
Error: auto_probe failed
&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't understand why I have this error message because when I do the exact same operation with the MKW21, MKW22 and the MK22FX512 (the other MCUs used by my company, I can flash the memory...)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is this SDID ? What does it mean ? Do I miss a configuration file or something ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Matthieu.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Dec 2017 12:58:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-use-OpenOCD-with-MKW24-Kinetis-MCU/m-p/763353#M46491</guid>
      <dc:creator>matthieuremacle</dc:creator>
      <dc:date>2017-12-05T12:58:22Z</dc:date>
    </item>
    <item>
      <title>Re: Can't use OpenOCD with MKW24 Kinetis MCU</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-use-OpenOCD-with-MKW24-Kinetis-MCU/m-p/763354#M46492</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Matthieu.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which flash programmer or IDE do you used ?&lt;/P&gt;&lt;P&gt;Have you select the right chip configuration when flash ?&lt;/P&gt;&lt;P&gt;And what about the debug interface inside OpenOCD， check it in the Device Manager :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2564iCB660114D7C5C491/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Dec 2017 09:53:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-t-use-OpenOCD-with-MKW24-Kinetis-MCU/m-p/763354#M46492</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-12-07T09:53:42Z</dc:date>
    </item>
  </channel>
</rss>