<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Multiple ADC channel readings in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Multiple-ADC-channel-readings/m-p/763148#M46480</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is an application note &lt;A href="https://www.nxp.com/docs/en/application-note/AN4590.pdf"&gt;AN4590 &lt;/A&gt;using DMA to emulate ADC flexible scan mode and &lt;A href="https://www.nxp.com/docs/en/application-note-software/AN4590SW.zip"&gt;AN4590SW &lt;/A&gt;is the related software.&lt;/P&gt;&lt;P&gt;Wish it helps!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Figure 2. Example process flow.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18562i4D50B5CEE3BC7B9B/image-size/large?v=v2&amp;amp;px=999" role="button" title="Figure 2. Example process flow.PNG" alt="Figure 2. Example process flow.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Feb 2018 02:40:57 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2018-02-22T02:40:57Z</dc:date>
    <item>
      <title>Multiple ADC channel readings</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Multiple-ADC-channel-readings/m-p/763147#M46479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a MK22FN512 processor ( k22f family). My application requires me to monitor lot of sensors and I need to keep track of about 10 channels.But I guess K22 has 2 ADC modules with two channels each ( A and B) and only two sets of SC1 and Result registers.So if I use PDB to trigger ther modules max I can do is 4 channels. After that I will have to change the adc channels which are mapped by using channelconfig API before the next trigger to get the read the next set of sensores?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a better way of doing it.In short I need to read about 10 ADC channels using k22f.I have some wiggle room for the rate at which these sensors are updated.( mostly used for monitoring and not control)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Feb 2018 23:41:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Multiple-ADC-channel-readings/m-p/763147#M46479</guid>
      <dc:creator>sreejithmenon</dc:creator>
      <dc:date>2018-02-20T23:41:43Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple ADC channel readings</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Multiple-ADC-channel-readings/m-p/763148#M46480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is an application note &lt;A href="https://www.nxp.com/docs/en/application-note/AN4590.pdf"&gt;AN4590 &lt;/A&gt;using DMA to emulate ADC flexible scan mode and &lt;A href="https://www.nxp.com/docs/en/application-note-software/AN4590SW.zip"&gt;AN4590SW &lt;/A&gt;is the related software.&lt;/P&gt;&lt;P&gt;Wish it helps!&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Figure 2. Example process flow.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18562i4D50B5CEE3BC7B9B/image-size/large?v=v2&amp;amp;px=999" role="button" title="Figure 2. Example process flow.PNG" alt="Figure 2. Example process flow.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 02:40:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Multiple-ADC-channel-readings/m-p/763148#M46480</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2018-02-22T02:40:57Z</dc:date>
    </item>
  </channel>
</rss>