<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: C90TFS Flash driver on K66F in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/C90TFS-Flash-driver-on-K66F/m-p/760624#M46367</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you have already experience you can erase/program in block 0 as long as you disable interrupts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need to do it without disabling interrupts you need to ensure that none of the interrupts that can be called will need to access block 0 (which can't be accessed during erase/programming operations). This can be done by having the interrupt vector table in SRAM (of the other half of Flash) and all possible code that will be executed in the interrupt in either SRAM or the other half of Flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Mar 2018 22:01:08 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2018-03-15T22:01:08Z</dc:date>
    <item>
      <title>C90TFS Flash driver on K66F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/C90TFS-Flash-driver-on-K66F/m-p/760623#M46366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using "MK66FN2M0VLQ18" for my controller.&lt;/P&gt;&lt;P&gt;1) If my program is running in the first 256K range, I am trying to erase/program from 0x0004_0000 to 0x0007_FFFF, I get MCU RESET. It works fine if I disable interrupt during flash operation.&lt;/P&gt;&lt;P&gt;2)&amp;nbsp;If I&amp;nbsp;&amp;nbsp;am trying to erase/program from 0x0008_0000 to 0x001F_FFFF, it works fine. no need to disable interrupt.&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;P&gt;1) Can I run a program in block0 and erase/program area in block0 as well? Or I have to erase/program in other block?&lt;/P&gt;&lt;P&gt;2) If need to erase/program in other block, why does it work if I disable the interrupt?&lt;/P&gt;&lt;P&gt;3) Is there any way to erase/program in the same block as running block? Do I need to set callback function to fix it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Mar 2018 15:50:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/C90TFS-Flash-driver-on-K66F/m-p/760623#M46366</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2018-03-15T15:50:09Z</dc:date>
    </item>
    <item>
      <title>Re: C90TFS Flash driver on K66F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/C90TFS-Flash-driver-on-K66F/m-p/760624#M46367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you have already experience you can erase/program in block 0 as long as you disable interrupts.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need to do it without disabling interrupts you need to ensure that none of the interrupts that can be called will need to access block 0 (which can't be accessed during erase/programming operations). This can be done by having the interrupt vector table in SRAM (of the other half of Flash) and all possible code that will be executed in the interrupt in either SRAM or the other half of Flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Mar 2018 22:01:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/C90TFS-Flash-driver-on-K66F/m-p/760624#M46367</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-03-15T22:01:08Z</dc:date>
    </item>
    <item>
      <title>Re: C90TFS Flash driver on K66F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/C90TFS-Flash-driver-on-K66F/m-p/760625#M46368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked C90TFS flash driver, there is option to run in RAM.&lt;/P&gt;&lt;P&gt;Could you tell me how to use this feature in C90TFS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Mar 2018 11:58:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/C90TFS-Flash-driver-on-K66F/m-p/760625#M46368</guid>
      <dc:creator>a8Chcx</dc:creator>
      <dc:date>2018-03-16T11:58:43Z</dc:date>
    </item>
    <item>
      <title>Re: C90TFS Flash driver on K66F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/C90TFS-Flash-driver-on-K66F/m-p/760626#M46369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't know of use the C90TFS driver so you will need to read its documentation for details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, it is always necessary to use SRAM to run the flashing code when working in the&amp;nbsp;same block as the code is in (if it worked by disabling interrupts for you I assume that it is already enabled).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Generally though the flash driver is only a part of the overall&amp;nbsp;solution - it won't solve details about where code is located and whether interrupts can be handled during flash operations; this is a system-wide design point beyond the driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Mar 2018 16:15:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/C90TFS-Flash-driver-on-K66F/m-p/760626#M46369</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-03-16T16:15:05Z</dc:date>
    </item>
  </channel>
</rss>