<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: MK66FN2M0VLQ18 ADC DIFF. Inputs</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66FN2M0VLQ18-ADC-DIFF-Inputs/m-p/759365#M46269</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000;"&gt;Hello, John&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000;"&gt;Yes, the datasheet is correct. That means actually o&lt;/SPAN&gt;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;nly one differential ADC input pair is available for K66, however you could use an external analog multiplexer to extend this capability. You may know from the datasheet that t&lt;/SPAN&gt;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;he inputs are&amp;nbsp;ADC0_DP3 and ADC0_DM3 for ADC0 channel 3 and&amp;nbsp;ADC1_DP0 and ADC1_DM0 for ADC1. They are shared same pins, so only one&amp;nbsp;&lt;SPAN&gt;differential ADC input pair&amp;nbsp;is available to use.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Apr 2018 07:36:19 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2018-04-25T07:36:19Z</dc:date>
    <item>
      <title>MK66FN2M0VLQ18 ADC DIFF. Inputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66FN2M0VLQ18-ADC-DIFF-Inputs/m-p/759364#M46268</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about the&amp;nbsp;MK66FN2M0VLQ18s ADC. I am using an applications that requires at least 2 but possibly 3 differential ADC Inputs. The&amp;nbsp;MK66FN2M0VLQ18 reference manual eludes to there being up to 4 differential ADC inputs but the MK66FN2M0VLQ18 datasheet&amp;nbsp;&amp;nbsp;has only 3 pins labels with DM marker and one is an overlap between the two diffent input channels, meaning I can at best only use one differential ADC input. Is this right or is there something I am missing like some of the single ended inputs can be used as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;John&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Apr 2018 18:34:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66FN2M0VLQ18-ADC-DIFF-Inputs/m-p/759364#M46268</guid>
      <dc:creator>johncooper</dc:creator>
      <dc:date>2018-04-23T18:34:30Z</dc:date>
    </item>
    <item>
      <title>Re: MK66FN2M0VLQ18 ADC DIFF. Inputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66FN2M0VLQ18-ADC-DIFF-Inputs/m-p/759365#M46269</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000;"&gt;Hello, John&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000;"&gt;Yes, the datasheet is correct. That means actually o&lt;/SPAN&gt;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;nly one differential ADC input pair is available for K66, however you could use an external analog multiplexer to extend this capability. You may know from the datasheet that t&lt;/SPAN&gt;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;he inputs are&amp;nbsp;ADC0_DP3 and ADC0_DM3 for ADC0 channel 3 and&amp;nbsp;ADC1_DP0 and ADC1_DM0 for ADC1. They are shared same pins, so only one&amp;nbsp;&lt;SPAN&gt;differential ADC input pair&amp;nbsp;is available to use.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2018 07:36:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK66FN2M0VLQ18-ADC-DIFF-Inputs/m-p/759365#M46269</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2018-04-25T07:36:19Z</dc:date>
    </item>
  </channel>
</rss>