<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: How do 32bit addresses map to K66 SDRAM address pins</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-32bit-addresses-map-to-K66-SDRAM-address-pins/m-p/757643#M46189</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jim,&lt;/P&gt;&lt;P&gt;As you know that the SDRAM is connected to K65/66 via SDRAM controller, the SDRAM controller can generate the corresponding Column address and Row address to access SDRAM if the space is in the SDRAM range. For K65, the 0x8000_0000–0x8FFF_FFFF is SDRAM address space, after the SDRAM is initialized, when you access the above space, the SDRAM will generate the timing to access SDRAM, you can access the SDRAM&amp;nbsp; as you access the internal SRAM, you do not need consider the precharge/activate/refresh...&lt;/P&gt;&lt;P&gt;I do not know if you ask the connection between SDRAM and SDRAM controller, based on SDRAM chip column address and data width(32 bits/16 bits/8 bits), the K65 provides several tables, which tell you how to connect the address between SDRAM controller address and SDRAM address.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Nov 2017 02:13:31 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2017-11-08T02:13:31Z</dc:date>
    <item>
      <title>How do 32bit addresses map to K66 SDRAM address pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-32bit-addresses-map-to-K66-SDRAM-address-pins/m-p/757642#M46188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the K66 and K65 MCUs, how does a 32bit address in an instruction get translated to the SDRAM controller address pins A23-A9?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Nov 2017 19:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-32bit-addresses-map-to-K66-SDRAM-address-pins/m-p/757642#M46188</guid>
      <dc:creator>jch4416</dc:creator>
      <dc:date>2017-11-07T19:22:35Z</dc:date>
    </item>
    <item>
      <title>Re: How do 32bit addresses map to K66 SDRAM address pins</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-32bit-addresses-map-to-K66-SDRAM-address-pins/m-p/757643#M46189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Jim,&lt;/P&gt;&lt;P&gt;As you know that the SDRAM is connected to K65/66 via SDRAM controller, the SDRAM controller can generate the corresponding Column address and Row address to access SDRAM if the space is in the SDRAM range. For K65, the 0x8000_0000–0x8FFF_FFFF is SDRAM address space, after the SDRAM is initialized, when you access the above space, the SDRAM will generate the timing to access SDRAM, you can access the SDRAM&amp;nbsp; as you access the internal SRAM, you do not need consider the precharge/activate/refresh...&lt;/P&gt;&lt;P&gt;I do not know if you ask the connection between SDRAM and SDRAM controller, based on SDRAM chip column address and data width(32 bits/16 bits/8 bits), the K65 provides several tables, which tell you how to connect the address between SDRAM controller address and SDRAM address.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Nov 2017 02:13:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-32bit-addresses-map-to-K66-SDRAM-address-pins/m-p/757643#M46189</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-11-08T02:13:31Z</dc:date>
    </item>
  </channel>
</rss>