<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックPreferred toolchain for FRDM-K28F board?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Preferred-toolchain-for-FRDM-K28F-board/m-p/756988#M46144</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I have a new FRDM-K28F board.&amp;nbsp; I am looking for an IDE that will allow setting of breakpoints and single step debugging (e.g. something Eclipse based) and a toolchain that will also allow CLI driven development of C code using Makefiles.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone suggest the best set of tools to achieve the above?&amp;nbsp; I've just downloaded MCU Expresso and wanted to try out a quick "hello world" demo, but when I click on "New Project" only the LPC based boards are listed.&amp;nbsp; I was hoping to load some ready to go samples for my FRDM board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On a higher level, since the NXP takeover should I be looking at using NXP chips now instead of Freescale?&amp;nbsp; I have a new design coming up and there's nothing at this point locking me into a particular vendor.&amp;nbsp; If support on the software side is going to focus mainly on NXP chips then it'd prob. make sense to just focus on that silicon from now on?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sean&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 22 Apr 2018 17:22:33 GMT</pubDate>
    <dc:creator>fastwalker2</dc:creator>
    <dc:date>2018-04-22T17:22:33Z</dc:date>
    <item>
      <title>Preferred toolchain for FRDM-K28F board?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Preferred-toolchain-for-FRDM-K28F-board/m-p/756988#M46144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;I have a new FRDM-K28F board.&amp;nbsp; I am looking for an IDE that will allow setting of breakpoints and single step debugging (e.g. something Eclipse based) and a toolchain that will also allow CLI driven development of C code using Makefiles.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone suggest the best set of tools to achieve the above?&amp;nbsp; I've just downloaded MCU Expresso and wanted to try out a quick "hello world" demo, but when I click on "New Project" only the LPC based boards are listed.&amp;nbsp; I was hoping to load some ready to go samples for my FRDM board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On a higher level, since the NXP takeover should I be looking at using NXP chips now instead of Freescale?&amp;nbsp; I have a new design coming up and there's nothing at this point locking me into a particular vendor.&amp;nbsp; If support on the software side is going to focus mainly on NXP chips then it'd prob. make sense to just focus on that silicon from now on?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sean&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Apr 2018 17:22:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Preferred-toolchain-for-FRDM-K28F-board/m-p/756988#M46144</guid>
      <dc:creator>fastwalker2</dc:creator>
      <dc:date>2018-04-22T17:22:33Z</dc:date>
    </item>
    <item>
      <title>Re: Preferred toolchain for FRDM-K28F board?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Preferred-toolchain-for-FRDM-K28F-board/m-p/756989#M46145</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sean&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;For MCUXpresso see the following: &lt;/SPAN&gt;&lt;A class="jive-link-thread-small" data-containerid="2019" data-containertype="14" data-objectid="474390" data-objecttype="1" href="https://community.nxp.com/thread/474390"&gt;https://community.nxp.com/thread/474390&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Also take a look at &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis%2FFRDM-KL28Z.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/kinetis/FRDM-KL28Z.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The uTasker KL28 project includes complete projects for most IDEs:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; NXP's MCUXpresso&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; NXP's Kinetis Design Studio (KDS)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Freescale's CodeWarrior 10.x&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; S32 Design Studio for ARM&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Rowley Associate's Crossworks&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CooCox CoIDE&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; IAR Embedded Workbench&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Keil µVision&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Green Hills&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Atollic TrueSTUDIO for ARM&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Standalone GCC from Makefile&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; VisualStudio for Kinetis simulation&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and allows complete project simulation (including peripherals, interrupt, DMA etc.) and CGG make file building directly from Visual Studio.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Beware however that the KL28 presently has a lead time of about 40 weeks so you will may need to keep your options open if you need to produce fast turnaround developments.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"NXP = Freescale" so there is no general problem with Kinetis parts (NXP is, or will be, Qualcomm - and Broadcom is also biding on Qualcomm, so best close your eyes if stability is an input to your choice of silicon)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;SPAN&gt;Kinetis: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Apr 2018 00:59:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Preferred-toolchain-for-FRDM-K28F-board/m-p/756989#M46145</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-04-23T00:59:01Z</dc:date>
    </item>
  </channel>
</rss>