<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: EA 24-bit SPI in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/EA-24-bit-SPI/m-p/756892#M46138</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robert，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Do you use both the KEA as SPI master and slave?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; In the Slave side, please enable the SSEL function, don't do it like master.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Jun 2018 03:04:42 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2018-06-08T03:04:42Z</dc:date>
    <item>
      <title>EA 24-bit SPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/EA-24-bit-SPI/m-p/756889#M46135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to work with 24-bit words via the SPI port on the KEA64? I am able to read 24-bits no problem, but when I send, there is always a clock cycle break between bytes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this is possible, then I will try harder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 21:15:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/EA-24-bit-SPI/m-p/756889#M46135</guid>
      <dc:creator>rmaier</dc:creator>
      <dc:date>2018-06-06T21:15:59Z</dc:date>
    </item>
    <item>
      <title>Re: EA 24-bit SPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/EA-24-bit-SPI/m-p/756890#M46136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robert,&lt;/P&gt;&lt;P&gt;&amp;nbsp; It's easy to realize it, just don't use the hardware SPI SSEL function.&lt;/P&gt;&lt;P&gt;&amp;nbsp; Use the GPIO function instead of the hardware SPI ssel function.&lt;/P&gt;&lt;P&gt;&amp;nbsp; You can configure C2[MODFEN] as 0:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26233i4EE3F1E510E205B6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Or you also can use the other GPIO pin as the SSEL pin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Before your send the SPI data, pull the SSEL low at first, after the SPI data send finished, then pull the SSEL high.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 05:52:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/EA-24-bit-SPI/m-p/756890#M46136</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-06-07T05:52:50Z</dc:date>
    </item>
    <item>
      <title>Re: EA 24-bit SPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/EA-24-bit-SPI/m-p/756891#M46137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kerry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the sanity check. I was able to make it work. Now, I just can't clear any faults on the slave. It looks like the message is sent nicely on the oscilloscope. The Kinetis is working just fine, I think I need to sort out some things on the slave side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 13:29:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/EA-24-bit-SPI/m-p/756891#M46137</guid>
      <dc:creator>rmaier</dc:creator>
      <dc:date>2018-06-07T13:29:34Z</dc:date>
    </item>
    <item>
      <title>Re: EA 24-bit SPI</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/EA-24-bit-SPI/m-p/756892#M46138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Robert，&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Do you use both the KEA as SPI master and slave?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; In the Slave side, please enable the SSEL function, don't do it like master.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jun 2018 03:04:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/EA-24-bit-SPI/m-p/756892#M46138</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-06-08T03:04:42Z</dc:date>
    </item>
  </channel>
</rss>