<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Problem with NRF24l01+, Status register</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-NRF24l01-Status-register/m-p/755277#M46072</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got problem with nRF24l01 modul. The SPI communications works, but when I&amp;nbsp; send payload (I only use transmmiter)I check the STATUS register and the value should be 0x10 for max retransmit payload, but it always set on 0x0E. What can be the problem ? Iam using KL25Z&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Code is below&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 21 Apr 2018 08:36:02 GMT</pubDate>
    <dc:creator>peteros</dc:creator>
    <dc:date>2018-04-21T08:36:02Z</dc:date>
    <item>
      <title>Problem with NRF24l01+, Status register</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-NRF24l01-Status-register/m-p/755277#M46072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got problem with nRF24l01 modul. The SPI communications works, but when I&amp;nbsp; send payload (I only use transmmiter)I check the STATUS register and the value should be 0x10 for max retransmit payload, but it always set on 0x0E. What can be the problem ? Iam using KL25Z&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Code is below&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Apr 2018 08:36:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-NRF24l01-Status-register/m-p/755277#M46072</guid>
      <dc:creator>peteros</dc:creator>
      <dc:date>2018-04-21T08:36:02Z</dc:date>
    </item>
  </channel>
</rss>