<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FRDM-KEAZ128 debug mode in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEAZ128-debug-mode/m-p/755231#M46065</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;没有12V真的可以吗？我现在仅仅用USB来供电，但是你发的例程，CAN信号就是出不来。我看了一下开发板的原理图。J107这个地方，如果接通23那么就是USB给单片机供电。如果接通12，那么就是SBC给单片机供电。也就是如果没有12V，那么SBC是没有电的，那么CAN收发器也就用不了。我是这样理解的。你可以去掉12V，仅仅用USB供电，然后试一下。如果能用的话，你拍个照片，我看看你开发板是怎么设置的。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Jun 2018 08:28:16 GMT</pubDate>
    <dc:creator>283230333</dc:creator>
    <dc:date>2018-06-07T08:28:16Z</dc:date>
    <item>
      <title>FRDM-KEAZ128 debug mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEAZ128-debug-mode/m-p/755227#M46061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a FRDM-KEAZ128 development board （part number FRDM-KEAZ128Q80）. There is a MC33903 SBC chip on the development board. I want to develop CAN now, but I don't want to configure the MC33903. I noticed that the MC33903 has a debug mode and can use the CAN transceiver without configuring the MC33903 via SPI. How to configure the circuit in the picture?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21010iCC6981BA17D3D782/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 13:51:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEAZ128-debug-mode/m-p/755227#M46061</guid>
      <dc:creator>283230333</dc:creator>
      <dc:date>2018-06-06T13:51:26Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KEAZ128 debug mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEAZ128-debug-mode/m-p/755228#M46062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Logan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; If you want to configure the MC33903 in debug mode, you need to follow that chip's datasheet:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/26475i19252A03153D2E26/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I suggest you control the SPI interface to enable the CAN module.&lt;/P&gt;&lt;P&gt;Actually, in the community, there has a sample code for your reference, you can refer to it:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/453806"&gt;FRDM-KEAZ128Q80 MSCAN Communication&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial, sans-serif; font-size: small;"&gt;&lt;A _jive_internal="true" data-content-finding="Community" href="https://community.nxp.com/servlet/JiveServlet/download/918307-1-405918/MSCAN_Driver FRDM_KEA128 Example_TransmitPerSecond.zip"&gt;MSCAN_Driver+FRDM_KEA128 Example_TransmitPerSecond.zip&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;It is &lt;SPAN style="font-family: Arial, sans-serif; font-size: small;"&gt;S32DS on FRDM-KEAZ128 board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial, sans-serif; font-size: small;"&gt;You can try this code:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 06:14:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEAZ128-debug-mode/m-p/755228#M46062</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-06-07T06:14:58Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KEAZ128 debug mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEAZ128-debug-mode/m-p/755229#M46063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does it need to connect 12V power at J16? &amp;nbsp;I don't have 12v power supply ，&amp;nbsp;I only have the USB interface .&amp;nbsp;Is this okay？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 06:48:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEAZ128-debug-mode/m-p/755229#M46063</guid>
      <dc:creator>283230333</dc:creator>
      <dc:date>2018-06-07T06:48:40Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KEAZ128 debug mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEAZ128-debug-mode/m-p/755230#M46064</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Logan,&lt;/P&gt;&lt;P&gt;&amp;nbsp; Yes, you are right, this board need to connect 12V power at J16, J107 need to connect pin1,2.&lt;/P&gt;&lt;P&gt;&amp;nbsp; The bit rate is 500Kpbs, this is my test result:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32575i4C472B14497CF005/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/32519iAF71FE5D4D27E00F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Actually, 12V power is very easy to find.&lt;/P&gt;&lt;P&gt;If you don't want to use 12V, you also can use our TRK-KEA128 board, that board CAN transiver don't need the external 12V, just USB cable is OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 08:21:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEAZ128-debug-mode/m-p/755230#M46064</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-06-07T08:21:14Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KEAZ128 debug mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEAZ128-debug-mode/m-p/755231#M46065</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;没有12V真的可以吗？我现在仅仅用USB来供电，但是你发的例程，CAN信号就是出不来。我看了一下开发板的原理图。J107这个地方，如果接通23那么就是USB给单片机供电。如果接通12，那么就是SBC给单片机供电。也就是如果没有12V，那么SBC是没有电的，那么CAN收发器也就用不了。我是这样理解的。你可以去掉12V，仅仅用USB供电，然后试一下。如果能用的话，你拍个照片，我看看你开发板是怎么设置的。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 08:28:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEAZ128-debug-mode/m-p/755231#M46065</guid>
      <dc:creator>283230333</dc:creator>
      <dc:date>2018-06-07T08:28:16Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KEAZ128 debug mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEAZ128-debug-mode/m-p/755232#M46066</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;在FRDM-KEA128板子上，没有12V真的不可以！&lt;/P&gt;&lt;P&gt;我已经试过了，你看我上面的结果呢，USB不行的。&lt;/P&gt;&lt;P&gt;所以我建议你，如果想只用USB，你用TRK-KEA128，那个板子的外部CAN收发器控制很简单，只控制CAN数据收发就行了。&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 09:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-KEAZ128-debug-mode/m-p/755232#M46066</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-06-07T09:03:08Z</dc:date>
    </item>
  </channel>
</rss>