<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KV58 RMII_REF_CLK source</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV58-RMII-REF-CLK-source/m-p/755197#M46060</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, we tried with the same clock config as the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;TWR-KV58 and it seems to work.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;The mcuexpresso clock configuration tool may need updating, as it uses the datasheet max EXTAL frequency of 48MHz, so won't let you specify 50MHz external clock.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Mar 2018 14:27:42 GMT</pubDate>
    <dc:creator>rowangifford</dc:creator>
    <dc:date>2018-03-14T14:27:42Z</dc:date>
    <item>
      <title>KV58 RMII_REF_CLK source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV58-RMII-REF-CLK-source/m-p/755195#M46058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The RMII interfaces requires 50Mhz clock source, we use a PHY which provides this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reference manual says &lt;EM&gt;the RMII clock source can be EXTAL clock or ENET_1588_CLKIN selected via SIM_SOPT2[RMIISRC]&amp;nbsp;&lt;/EM&gt; (page 172), so we have routed the PHY clock source to the EXTAL pin and configured&amp;nbsp;&lt;EM&gt;SIM_SOPT2&amp;nbsp;&lt;/EM&gt;to use EXTAL as a source.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However datasheet section&lt;EM&gt; 3.3.2.2 Oscillator frequency specifications&amp;nbsp;&lt;/EM&gt;states&amp;nbsp;fec_extal&amp;nbsp;Input clock frequency (external clock mode) to be 48Mhz max.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So can a 50Mhz clock source be fed into EXTAL input, or is&amp;nbsp;ENET_1588_CLKIN&amp;nbsp;the only valid RMII clock source?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Rowan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Mar 2018 17:28:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV58-RMII-REF-CLK-source/m-p/755195#M46058</guid>
      <dc:creator>rowangifford</dc:creator>
      <dc:date>2018-03-13T17:28:15Z</dc:date>
    </item>
    <item>
      <title>Re: KV58 RMII_REF_CLK source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV58-RMII-REF-CLK-source/m-p/755196#M46059</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Rowan,&lt;/P&gt;&lt;P&gt;I have seen the maximum value 48MHz for Input clock frequency (external clock mode) exactly on data sheet of KV58, I do not know the background of the spec.&lt;/P&gt;&lt;P&gt;But we connect 50mhz clock signal to Extal pin for KV58, no problem.&lt;/P&gt;&lt;P&gt;This is the input clock circuit on TWR-KV58:&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22948iE4EB836AEC66668B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Mar 2018 04:19:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV58-RMII-REF-CLK-source/m-p/755196#M46059</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-03-14T04:19:04Z</dc:date>
    </item>
    <item>
      <title>Re: KV58 RMII_REF_CLK source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV58-RMII-REF-CLK-source/m-p/755197#M46060</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, we tried with the same clock config as the&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;TWR-KV58 and it seems to work.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;The mcuexpresso clock configuration tool may need updating, as it uses the datasheet max EXTAL frequency of 48MHz, so won't let you specify 50MHz external clock.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Mar 2018 14:27:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KV58-RMII-REF-CLK-source/m-p/755197#M46060</guid>
      <dc:creator>rowangifford</dc:creator>
      <dc:date>2018-03-14T14:27:42Z</dc:date>
    </item>
  </channel>
</rss>