<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックCan we use MK66FN2M0VLQ18 as a drop-in replacement for MK60FN1M0VLQ12 ?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-MK66FN2M0VLQ18-as-a-drop-in-replacement-for/m-p/754741#M46028</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using&amp;nbsp;MK60FN1M0VLQ12 (1 MB Internal Flash and 128 KB Internal SRAM) now in a product.&lt;/P&gt;&lt;P&gt;We plan to change it to&amp;nbsp;MK66FN2M0VLQ18 &lt;SPAN&gt;(2 MB&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Internal&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN&gt;Flash and&amp;nbsp;256 KB Internal&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN&gt;SRAM&lt;/SPAN&gt;&lt;SPAN&gt;)&amp;nbsp;&lt;/SPAN&gt;to increase the size of Internal Flash and SRAM.&lt;/P&gt;&lt;P&gt;Will it be a drop-in replacement without any Hardware redesign?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Nov 2017 08:43:17 GMT</pubDate>
    <dc:creator>sankarunnikrish</dc:creator>
    <dc:date>2017-11-07T08:43:17Z</dc:date>
    <item>
      <title>Can we use MK66FN2M0VLQ18 as a drop-in replacement for MK60FN1M0VLQ12 ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-MK66FN2M0VLQ18-as-a-drop-in-replacement-for/m-p/754741#M46028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using&amp;nbsp;MK60FN1M0VLQ12 (1 MB Internal Flash and 128 KB Internal SRAM) now in a product.&lt;/P&gt;&lt;P&gt;We plan to change it to&amp;nbsp;MK66FN2M0VLQ18 &lt;SPAN&gt;(2 MB&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Internal&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN&gt;Flash and&amp;nbsp;256 KB Internal&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN&gt;SRAM&lt;/SPAN&gt;&lt;SPAN&gt;)&amp;nbsp;&lt;/SPAN&gt;to increase the size of Internal Flash and SRAM.&lt;/P&gt;&lt;P&gt;Will it be a drop-in replacement without any Hardware redesign?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Nov 2017 08:43:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-MK66FN2M0VLQ18-as-a-drop-in-replacement-for/m-p/754741#M46028</guid>
      <dc:creator>sankarunnikrish</dc:creator>
      <dc:date>2017-11-07T08:43:17Z</dc:date>
    </item>
    <item>
      <title>Re: Can we use MK66FN2M0VLQ18 as a drop-in replacement for MK60FN1M0VLQ12 ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-MK66FN2M0VLQ18-as-a-drop-in-replacement-for/m-p/754742#M46029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sankar&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K66 in 144 LQFP can be placed on the footprint of a K60 since its power supply pins are the same.&lt;BR /&gt;However, whether it can used directly depends on the design.&lt;/P&gt;&lt;P&gt;For example, if you presently use high speed USB on the K60, connected via ULPI it won't operate the same - the K66 doesn't use this interface and has an internal HW USB transceiver, making the overall circuit different and incompatible.&lt;/P&gt;&lt;P&gt;The same is true for several peripheral functions: eg, if you presently use I2S on PTE24 it is not available in the K66.&lt;BR /&gt;The K66 also has no NAND controller, in case this is used in your present design.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that there are quite a number of SW differences between the two devices (eg. LPUARTs replace some UARTs even when the pin outs are essentially compatible).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To summarise, it is true to say that there is a high level of HW compatibility which makes a replacement possible in some cases. However it still depends on the present design as to what exactly needs to work and there is a risk that something will no longer be possible. You need to check each pin functionality between the two to be ale to decide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Nov 2017 09:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Can-we-use-MK66FN2M0VLQ18-as-a-drop-in-replacement-for/m-p/754742#M46029</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2017-11-07T09:47:54Z</dc:date>
    </item>
  </channel>
</rss>