<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic mqx for kinetis k20 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mqx-for-kinetis-k20/m-p/227260#M4602</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;I am currently working on a project, where&amp;nbsp; I have to handle several real time data. I am using k20 to achieve the target.&lt;/P&gt;&lt;P&gt;I am getting in dealing with all these interrupts. So thought to implement mqx rtos in the project.&lt;/P&gt;&lt;P&gt;Can anyone suggest me whether it is feasible to use mqx with k20.&lt;/P&gt;&lt;P&gt;In the project i am dealing with these peripherals:&lt;/P&gt;&lt;P&gt;-dma&lt;/P&gt;&lt;P&gt;-gpio&lt;/P&gt;&lt;P&gt;-can&lt;/P&gt;&lt;P&gt;-usb-otg&lt;/P&gt;&lt;P&gt;-serial&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Gagan Garg &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 May 2013 10:25:20 GMT</pubDate>
    <dc:creator>gagangarg</dc:creator>
    <dc:date>2013-05-07T10:25:20Z</dc:date>
    <item>
      <title>mqx for kinetis k20</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mqx-for-kinetis-k20/m-p/227260#M4602</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;I am currently working on a project, where&amp;nbsp; I have to handle several real time data. I am using k20 to achieve the target.&lt;/P&gt;&lt;P&gt;I am getting in dealing with all these interrupts. So thought to implement mqx rtos in the project.&lt;/P&gt;&lt;P&gt;Can anyone suggest me whether it is feasible to use mqx with k20.&lt;/P&gt;&lt;P&gt;In the project i am dealing with these peripherals:&lt;/P&gt;&lt;P&gt;-dma&lt;/P&gt;&lt;P&gt;-gpio&lt;/P&gt;&lt;P&gt;-can&lt;/P&gt;&lt;P&gt;-usb-otg&lt;/P&gt;&lt;P&gt;-serial&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Gagan Garg &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2013 10:25:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mqx-for-kinetis-k20/m-p/227260#M4602</guid>
      <dc:creator>gagangarg</dc:creator>
      <dc:date>2013-05-07T10:25:20Z</dc:date>
    </item>
    <item>
      <title>Re: mqx for kinetis k20</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mqx-for-kinetis-k20/m-p/227261#M4603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, MQX would work well for you in this scenario running on a K20. More importantly, which version of the K20 are you running? The silicon version (50MHz, 72MHz, 100MHz, etc...) is more important for starting your MQX port than is the K20 designation. A K20 100 MHz part is more closely related to a K40 100 MHz part than it is to a K20 50 MHz part. The "20" is more telling of the peripheral set of the part than it is of the silicon.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 May 2013 12:15:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mqx-for-kinetis-k20/m-p/227261#M4603</guid>
      <dc:creator>dspNeil</dc:creator>
      <dc:date>2013-05-07T12:15:33Z</dc:date>
    </item>
  </channel>
</rss>