<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: mkw31Z semihosting not working</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mkw31Z-semihosting-not-working/m-p/753482#M45931</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Frank Strazzabosco&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the following post:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2016/08/06/semihosting-again-with-nxp-kinetis-sdk-v2-0/" title="https://mcuoneclipse.com/2016/08/06/semihosting-again-with-nxp-kinetis-sdk-v2-0/"&gt;Semihosting (again!) with NXP Kinetis SDK V2.0 | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have the telnet port with 2333?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, there are some bugs and errors that have been fixed in the new wireless stack, which is supported with MCUXpresso IDE, where the semihosting is already implemented as a part of the configuration, so I would like to recommend you to migrate to MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 09 Dec 2017 00:23:23 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2017-12-09T00:23:23Z</dc:date>
    <item>
      <title>mkw31Z semihosting not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mkw31Z-semihosting-not-working/m-p/753481#M45930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using KDS version 3.2.0 and believe I had all the various things needed for semihosting a printf to the debugger console set.&lt;/P&gt;&lt;P&gt;The JLINK debugger has semihosting enabled in the startup &amp;amp; debuuger tabs of the config lauch&lt;/P&gt;&lt;P&gt;You can see the Semihosting and SWV thread is running in the deug window.&lt;/P&gt;&lt;P&gt;The console window is switched over to display the "SEGGER J-Link GBD Server V6.12d - Terminal output channel"&lt;/P&gt;&lt;P&gt;The linker is set to use the -specs=nano.specs -specs=rdimon.specs&lt;/P&gt;&lt;P&gt;The printf call returns fine after giving the build enough heap space but no characters appear in the KDS console window.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Nov 2017 22:48:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mkw31Z-semihosting-not-working/m-p/753481#M45930</guid>
      <dc:creator>microfirm</dc:creator>
      <dc:date>2017-11-30T22:48:04Z</dc:date>
    </item>
    <item>
      <title>Re: mkw31Z semihosting not working</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mkw31Z-semihosting-not-working/m-p/753482#M45931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Frank Strazzabosco&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the following post:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuoneclipse.com/2016/08/06/semihosting-again-with-nxp-kinetis-sdk-v2-0/" title="https://mcuoneclipse.com/2016/08/06/semihosting-again-with-nxp-kinetis-sdk-v2-0/"&gt;Semihosting (again!) with NXP Kinetis SDK V2.0 | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have the telnet port with 2333?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, there are some bugs and errors that have been fixed in the new wireless stack, which is supported with MCUXpresso IDE, where the semihosting is already implemented as a part of the configuration, so I would like to recommend you to migrate to MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Dec 2017 00:23:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mkw31Z-semihosting-not-working/m-p/753482#M45931</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-12-09T00:23:23Z</dc:date>
    </item>
  </channel>
</rss>