<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic UART 8N2 with MK02 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-8N2-with-MK02/m-p/753233#M45908</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had to note to my horror the MK02 supports no 2nd stop at UART. But I need it.&lt;BR /&gt;Is it possible to use the 9th bit at a 9bit transmission? I think it is but maybe not considered something. So better to ask.&lt;BR /&gt;I noticed also the 9bit transmission is not supported in the SDK. Is there a similar SDK what supports it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Marcus&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 17 Feb 2018 21:43:06 GMT</pubDate>
    <dc:creator>tirak</dc:creator>
    <dc:date>2018-02-17T21:43:06Z</dc:date>
    <item>
      <title>UART 8N2 with MK02</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-8N2-with-MK02/m-p/753233#M45908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had to note to my horror the MK02 supports no 2nd stop at UART. But I need it.&lt;BR /&gt;Is it possible to use the 9th bit at a 9bit transmission? I think it is but maybe not considered something. So better to ask.&lt;BR /&gt;I noticed also the 9bit transmission is not supported in the SDK. Is there a similar SDK what supports it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Marcus&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Feb 2018 21:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-8N2-with-MK02/m-p/753233#M45908</guid>
      <dc:creator>tirak</dc:creator>
      <dc:date>2018-02-17T21:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: UART 8N2 with MK02</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-8N2-with-MK02/m-p/753234#M45909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marcus Günther&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't see problem implementing this. Your ninth bit will represent your first stop bit. Some points to consider;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-You will not be able to enable parity&lt;/P&gt;&lt;P&gt;-When transmitting in 9-bit data format and using 8-bit write instructions, write first to transmit bit 8 in UART control register 3 (C3[T8]), then D.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, there isn't implemented 9bit for the sdk, you can setup this in the C1 register and writting the ninth C3[T8].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information helps you&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Feb 2018 00:28:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/UART-8N2-with-MK02/m-p/753234#M45909</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2018-02-23T00:28:56Z</dc:date>
    </item>
  </channel>
</rss>