<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 K28 Vrefh pin connection option</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K28-Vrefh-pin-connection-option/m-p/752425#M45835</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a design that is power sensitive put I also need accurate adc readings. For this reason I'm adding a external prec ref voltage source. I will not be doing measurements all the time and If I shut down the prec ref I can save about 100ua. The only issue is that the Vrefh pin into the micro will be floating. Will this be a issue? The data sheet says unused pins short go to VDD but what happens if I let it float? Since I will not be doing any reading I would think it should not be a issue. It will have a impedance to gnd through the prec ref chip. Would that be good or bad?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Feb 2018 21:32:12 GMT</pubDate>
    <dc:creator>jasonlarson</dc:creator>
    <dc:date>2018-02-16T21:32:12Z</dc:date>
    <item>
      <title>K28 Vrefh pin connection option</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K28-Vrefh-pin-connection-option/m-p/752425#M45835</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a design that is power sensitive put I also need accurate adc readings. For this reason I'm adding a external prec ref voltage source. I will not be doing measurements all the time and If I shut down the prec ref I can save about 100ua. The only issue is that the Vrefh pin into the micro will be floating. Will this be a issue? The data sheet says unused pins short go to VDD but what happens if I let it float? Since I will not be doing any reading I would think it should not be a issue. It will have a impedance to gnd through the prec ref chip. Would that be good or bad?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Feb 2018 21:32:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K28-Vrefh-pin-connection-option/m-p/752425#M45835</guid>
      <dc:creator>jasonlarson</dc:creator>
      <dc:date>2018-02-16T21:32:12Z</dc:date>
    </item>
    <item>
      <title>Re: K28 Vrefh pin connection option</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K28-Vrefh-pin-connection-option/m-p/752426#M45836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason,&lt;/P&gt;&lt;P&gt;I think it is ok if it float to ground. Please see&amp;nbsp; this link:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/419427?commentID=419427#comment-419427"&gt;https://community.nxp.com/message/419427?commentID=419427#comment-419427&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 06:34:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K28-Vrefh-pin-connection-option/m-p/752426#M45836</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2018-02-22T06:34:47Z</dc:date>
    </item>
  </channel>
</rss>