<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 K66 Pinout ADC0_DP0 not found</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Pinout-ADC0-DP0-not-found/m-p/751921#M45820</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use differential ADC in K66 uC, but I only found one of the two ADCs ports because the negative pair to use with pin 28 is not in the datasheet.&lt;/P&gt;&lt;P&gt;I have ADC0_DM0 or ADC1_DM3 on pin 28 (L2) but I cann`t find ADC0_DP0 or ADC1_DP3&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Feb 2018 12:00:04 GMT</pubDate>
    <dc:creator>jayas</dc:creator>
    <dc:date>2018-02-16T12:00:04Z</dc:date>
    <item>
      <title>K66 Pinout ADC0_DP0 not found</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Pinout-ADC0-DP0-not-found/m-p/751921#M45820</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use differential ADC in K66 uC, but I only found one of the two ADCs ports because the negative pair to use with pin 28 is not in the datasheet.&lt;/P&gt;&lt;P&gt;I have ADC0_DM0 or ADC1_DM3 on pin 28 (L2) but I cann`t find ADC0_DP0 or ADC1_DP3&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Feb 2018 12:00:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Pinout-ADC0-DP0-not-found/m-p/751921#M45820</guid>
      <dc:creator>jayas</dc:creator>
      <dc:date>2018-02-16T12:00:04Z</dc:date>
    </item>
    <item>
      <title>Re: K66 Pinout ADC0_DP0 not found</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Pinout-ADC0-DP0-not-found/m-p/751922#M45821</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Juan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the K66, the &lt;STRONG&gt;ADC0_DP0&lt;/STRONG&gt; is not available for differential inputs. Only the pins 29 and 30 can be used as differential inputs and are shared between ADC0 and ADC1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The inputs are&amp;nbsp;ADC0_DP3 and ADC0_DM3 for ADC0 channel 3 and&amp;nbsp;ADC1_DP0 and ADC1_DM0 for ADC1.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18711i9682D4FB7DD7B2A3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 24 Feb 2018 01:28:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Pinout-ADC0-DP0-not-found/m-p/751922#M45821</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2018-02-24T01:28:06Z</dc:date>
    </item>
    <item>
      <title>Re: K66 Pinout ADC0_DP0 not found</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Pinout-ADC0-DP0-not-found/m-p/751923#M45822</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Gerardo. It means than we can only use 1 differential ADC input un this model, isn't?&lt;/P&gt;&lt;P&gt;Only if we found an exernal multiplexing device to switch between channels we can use ADC0 and AD1 sharing same pins.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Feb 2018 16:10:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Pinout-ADC0-DP0-not-found/m-p/751923#M45822</guid>
      <dc:creator>jayas</dc:creator>
      <dc:date>2018-02-26T16:10:14Z</dc:date>
    </item>
    <item>
      <title>Re: K66 Pinout ADC0_DP0 not found</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Pinout-ADC0-DP0-not-found/m-p/751924#M45823</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Juan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is correct. Only one differential ADC input is available for the K66, but you could use an external analog multiplexer to extend this capability.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Feb 2018 22:18:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K66-Pinout-ADC0-DP0-not-found/m-p/751924#M45823</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2018-02-28T22:18:09Z</dc:date>
    </item>
  </channel>
</rss>