<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TWR K60D100M debugging sample example in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-debugging-sample-example/m-p/226580#M4573</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Girish, try uninstalling/reinstalling the twr drivers and using a different USB port on your computer, the OSJTAG drivers are located in the following directory:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Freescale\CW MCU v10.X\Drivers\P&amp;amp;E\Drivers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need to downgrade the firmware version in your TWR-K60 you need to use the P&amp;amp;E Firmware update and recovery utility, if you don't have it you can download it from this link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/osbdm/index.cfm" title="http://www.pemicro.com/osbdm/index.cfm"&gt;http://www.pemicro.com/osbdm/index.cfm&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Open the recovery utility and it will let you select the firmware file to flash the TWR.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Jan 2013 20:08:46 GMT</pubDate>
    <dc:creator>apanecatl</dc:creator>
    <dc:date>2013-01-16T20:08:46Z</dc:date>
    <item>
      <title>TWR K60D100M debugging sample example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-debugging-sample-example/m-p/226579#M4572</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was running in to problem while in debug mode with TWR-K60D100M. I used to get "Launch Error". &lt;/P&gt;&lt;P&gt;I also checked the Licensing information under the help and there appears no information &lt;/P&gt;&lt;P&gt;I recalled that TWR-K60N512 kit needs firmware update before updating. So I assumed that this kit would also need the same update.&lt;/P&gt;&lt;P&gt;After firmware update, the TWR-K60D100M appears as serial device on COM10. Before update it was appearing as USBCOM device.&lt;/P&gt;&lt;P&gt;The serial redirector utility available can support up to COM8. I am unable connect the tower kit to serial port anymore!&lt;/P&gt;&lt;P&gt;Could you suggest me how to roll back? I do not have the original bootloader form TWR-K60D100M.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After compiling the Hello project, I get following message:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Failed to resume target process., There was an error parsing the memory configuration file:&lt;/P&gt;&lt;P&gt;Can't open "MK60D10.mem" file&lt;/P&gt;&lt;P&gt; ("twrk60d100m.mem":20)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anyone suggest me what is this and is there problem with the setting or something?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Girish&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2013 15:00:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-debugging-sample-example/m-p/226579#M4572</guid>
      <dc:creator>GirishChoudanka</dc:creator>
      <dc:date>2013-01-16T15:00:58Z</dc:date>
    </item>
    <item>
      <title>Re: TWR K60D100M debugging sample example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-debugging-sample-example/m-p/226580#M4573</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Girish, try uninstalling/reinstalling the twr drivers and using a different USB port on your computer, the OSJTAG drivers are located in the following directory:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:\Freescale\CW MCU v10.X\Drivers\P&amp;amp;E\Drivers&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you need to downgrade the firmware version in your TWR-K60 you need to use the P&amp;amp;E Firmware update and recovery utility, if you don't have it you can download it from this link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/osbdm/index.cfm" title="http://www.pemicro.com/osbdm/index.cfm"&gt;http://www.pemicro.com/osbdm/index.cfm&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Open the recovery utility and it will let you select the firmware file to flash the TWR.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2013 20:08:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-K60D100M-debugging-sample-example/m-p/226580#M4573</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2013-01-16T20:08:46Z</dc:date>
    </item>
  </channel>
</rss>