<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CRC_CRC endianness dependent on CRC_CTRL[WAS]? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRC-CRC-endianness-dependent-on-CRC-CTRL-WAS/m-p/749093#M45604</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry for the late reply!&lt;/P&gt;&lt;P&gt;"However, when I write *data* values to CRC_CRC I must reverse it from LSB to MSB"&lt;BR /&gt;I don't think you have to reverse it from LSB to MSB, this hardware CRC module support Transpose feature.&lt;BR /&gt;Have you try to configure Types of transpose?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21401iEC6CBE18F83FA5EB/image-size/large?v=v2&amp;amp;px=999" title="Transpose feature.png" alt="Transpose feature.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;DIV&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Jun 2018 09:18:38 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2018-06-14T09:18:38Z</dc:date>
    <item>
      <title>CRC_CRC endianness dependent on CRC_CTRL[WAS]?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRC-CRC-endianness-dependent-on-CRC-CTRL-WAS/m-p/749092#M45603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I program the Kinetis K60 (little endian) via assembly.&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;"When programming data values, the values can be written 8 bits, 16 bits, or 32 bits at a&lt;BR /&gt;time, provided all bytes are contiguous; with *MSB* of data value written first."&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you write the *seed* value to CRC_CRC you MUST NOT reverse the byte order from LSB to MSB.&lt;/P&gt;&lt;P&gt;However, when I write *data* values to CRC_CRC I must reverse it from LSB to MSB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is that expected behavior?&lt;/P&gt;&lt;P&gt;Does the specification really distinguish between the terms "seed value" and "data value", so that the MSB restriction only applies to "data values"?&lt;/P&gt;&lt;P&gt;Would be quite confusing. Is there a reason?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 13 May 2018 09:23:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRC-CRC-endianness-dependent-on-CRC-CTRL-WAS/m-p/749092#M45603</guid>
      <dc:creator>xarowubas</dc:creator>
      <dc:date>2018-05-13T09:23:49Z</dc:date>
    </item>
    <item>
      <title>Re: CRC_CRC endianness dependent on CRC_CTRL[WAS]?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRC-CRC-endianness-dependent-on-CRC-CTRL-WAS/m-p/749093#M45604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry for the late reply!&lt;/P&gt;&lt;P&gt;"However, when I write *data* values to CRC_CRC I must reverse it from LSB to MSB"&lt;BR /&gt;I don't think you have to reverse it from LSB to MSB, this hardware CRC module support Transpose feature.&lt;BR /&gt;Have you try to configure Types of transpose?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21401iEC6CBE18F83FA5EB/image-size/large?v=v2&amp;amp;px=999" title="Transpose feature.png" alt="Transpose feature.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;DIV&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jun 2018 09:18:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CRC-CRC-endianness-dependent-on-CRC-CTRL-WAS/m-p/749093#M45604</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2018-06-14T09:18:38Z</dc:date>
    </item>
  </channel>
</rss>