<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKL03 DAC output pin for signal generation</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin-for-signal-generation/m-p/748810#M45595</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a very basic question. I want to generate a signal with the FRDM-KL03 board and give this generated analog waveform say to some external circuit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using KDS software and following the&lt;A href="http://www.utasker.com/docs/uTasker/uTaskerADC.pdf"&gt; ADC uTasker guide&amp;nbsp;&lt;/A&gt;(page 12).&lt;/P&gt;&lt;P&gt;Now, the Kinetis SDK Application User Guide says that: "Normally, the&amp;nbsp;DAC0_OUT is internally connected to the ADC0_SE23 (DAC0_OUT is a source of ADC0_SE23),".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, is the output of the DAC going in input to the ADC?&amp;nbsp;&lt;/P&gt;&lt;P&gt;And if I want to "see" the generated signal, to which jumper on the FRDM-KL03 board should I connect? From the &lt;A href="https://www.nxp.com/docs/en/reference-manual/KL03P24M48SF0RM.pdf"&gt;KL03 Sub-family manual&lt;/A&gt;&amp;nbsp;(table page 99) it&amp;nbsp;seems to be the J4-PTA9? But I am not sure. I mean I tried but I could not see the waveform&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Apr 2018 17:39:29 GMT</pubDate>
    <dc:creator>raff5184</dc:creator>
    <dc:date>2018-04-19T17:39:29Z</dc:date>
    <item>
      <title>KL03 DAC output pin for signal generation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin-for-signal-generation/m-p/748810#M45595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a very basic question. I want to generate a signal with the FRDM-KL03 board and give this generated analog waveform say to some external circuit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using KDS software and following the&lt;A href="http://www.utasker.com/docs/uTasker/uTaskerADC.pdf"&gt; ADC uTasker guide&amp;nbsp;&lt;/A&gt;(page 12).&lt;/P&gt;&lt;P&gt;Now, the Kinetis SDK Application User Guide says that: "Normally, the&amp;nbsp;DAC0_OUT is internally connected to the ADC0_SE23 (DAC0_OUT is a source of ADC0_SE23),".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, is the output of the DAC going in input to the ADC?&amp;nbsp;&lt;/P&gt;&lt;P&gt;And if I want to "see" the generated signal, to which jumper on the FRDM-KL03 board should I connect? From the &lt;A href="https://www.nxp.com/docs/en/reference-manual/KL03P24M48SF0RM.pdf"&gt;KL03 Sub-family manual&lt;/A&gt;&amp;nbsp;(table page 99) it&amp;nbsp;seems to be the J4-PTA9? But I am not sure. I mean I tried but I could not see the waveform&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2018 17:39:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin-for-signal-generation/m-p/748810#M45595</guid>
      <dc:creator>raff5184</dc:creator>
      <dc:date>2018-04-19T17:39:29Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 DAC output pin for signal generation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin-for-signal-generation/m-p/748811#M45596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;The KL03 has a 6 bit DAC in its comparator module and its output is not available on an external pin:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29023iE96CCE6B034D936D/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no 12 bit DAC as many other parts have which can be used for such functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, what you can do is use a PWM output with an RC filter to generate an analogue output signal or waveform.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;SPAN&gt;Kinetis: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2018 21:35:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin-for-signal-generation/m-p/748811#M45596</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-04-19T21:35:39Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 DAC output pin for signal generation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin-for-signal-generation/m-p/748812#M45597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Mark,&lt;/P&gt;&lt;P&gt;also would it be possible to do something like that with the GPIO?&amp;nbsp;&lt;BR /&gt;Basically I only need to generate a periodic square wave at very low frequencies, not even a sinusoid.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Apr 2018 22:00:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin-for-signal-generation/m-p/748812#M45597</guid>
      <dc:creator>raff5184</dc:creator>
      <dc:date>2018-04-20T22:00:46Z</dc:date>
    </item>
    <item>
      <title>Re: KL03 DAC output pin for signal generation</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin-for-signal-generation/m-p/748813#M45598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can generate square wave outputs (or PWM) with the TPM.&lt;BR /&gt;If you prefer to do it with timer interrupts toggling an GPIO output you can do it from the SYSTICK, TPM, PIT etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;SPAN&gt;Kinetis: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Apr 2018 01:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL03-DAC-output-pin-for-signal-generation/m-p/748813#M45598</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-04-23T01:01:55Z</dc:date>
    </item>
  </channel>
</rss>