<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using TWR-MEM MRAM with TWR-K53N512 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TWR-MEM-MRAM-with-TWR-K53N512/m-p/157022#M455</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Solved...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For anyone just starting out and running into this problem,&amp;nbsp;all the projects in KINETIS512_SC.zip are for IAR (v6.3 in the case of the platform I'm using). Once you have IAR going, just click example projects and direct it to the KINETIS512_SC directory. Build the project and change the settings for the debugger (if not using J-Link).&lt;BR /&gt;&lt;BR /&gt;Still not sure about power measurement...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Apr 2012 21:28:53 GMT</pubDate>
    <dc:creator>J_Hunt</dc:creator>
    <dc:date>2012-04-27T21:28:53Z</dc:date>
    <item>
      <title>Using TWR-MEM MRAM with TWR-K53N512</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TWR-MEM-MRAM-with-TWR-K53N512/m-p/157020#M453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am new to using the freescale architecture.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The setup I am working off is TWR-K53N512, TWR-MEM, TWR-SER, TWR-LCD.&amp;nbsp; All modules have default jumper settings except J16 on TWR-K53N512 to enable power via battery to memory.&amp;nbsp; I am working off of CodeWarrior 10.2 and got the projects from the KINETIS512_SC.zip.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to run the flexbus example to provide an example of how to interface with the MRAM.&amp;nbsp; As I understand it, the default jumper settings for both modules should allow for this project to be compiled and debugged via USB OSJTAG.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have gotten the project to build. When I try to run debug,&amp;nbsp; I use the following settings:&lt;/P&gt;&lt;P&gt;Project - k53-flexbus&lt;/P&gt;&lt;P&gt;Application - MK53N512CMD100_INTERNAL_RAM/k53-flexbus.afx&lt;/P&gt;&lt;P&gt;Build Configuration: MK53N512CMD100_INTERNAL_RAM&lt;/P&gt;&lt;P&gt;Use workspace settings (selected)&lt;/P&gt;&lt;P&gt;Connection - k53-hello-world_MK53N512CMD100_INTERNAL_RAM_PnE OSJTAG&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Once I hit Debug, the error I get is:&lt;/P&gt;&lt;P&gt;Failed to resume target process., There was an error parsing the memory configuration file: Can't open "MK53N512CMD100.mem" file &amp;nbsp;("MK53N512CMD100.mem":20)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am not sure if there is a&amp;nbsp;problem with building it using the&amp;nbsp;MK53N512CMD100_INTERNAL_RAM &amp;nbsp;realize that there probably should be a setting for MRAM, but the only options I see currently are either INTERNAL_RAM or INTERNAL_FLASH.&amp;nbsp; I am fairly certain that I am just missing something small here.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Summary&amp;nbsp;questions:&lt;/P&gt;&lt;P&gt;What am I doing incorrectly in getting this project to run on the platform?&lt;/P&gt;&lt;P&gt;Where can I find the drivers for the MRAM (if they are available)?&lt;/P&gt;&lt;P&gt;Is there any way to measure the power&amp;nbsp;used by&amp;nbsp;the MRAM on the&amp;nbsp;TWR-MEM?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2012 00:16:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TWR-MEM-MRAM-with-TWR-K53N512/m-p/157020#M453</guid>
      <dc:creator>J_Hunt</dc:creator>
      <dc:date>2012-04-25T00:16:59Z</dc:date>
    </item>
    <item>
      <title>Re: Using TWR-MEM MRAM with TWR-K53N512</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TWR-MEM-MRAM-with-TWR-K53N512/m-p/157021#M454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Question continuation:&lt;/P&gt;&lt;P&gt;Is there a way to measure the power used by MRAM via software?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Apr 2012 00:23:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TWR-MEM-MRAM-with-TWR-K53N512/m-p/157021#M454</guid>
      <dc:creator>J_Hunt</dc:creator>
      <dc:date>2012-04-25T00:23:16Z</dc:date>
    </item>
    <item>
      <title>Re: Using TWR-MEM MRAM with TWR-K53N512</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TWR-MEM-MRAM-with-TWR-K53N512/m-p/157022#M455</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Solved...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For anyone just starting out and running into this problem,&amp;nbsp;all the projects in KINETIS512_SC.zip are for IAR (v6.3 in the case of the platform I'm using). Once you have IAR going, just click example projects and direct it to the KINETIS512_SC directory. Build the project and change the settings for the debugger (if not using J-Link).&lt;BR /&gt;&lt;BR /&gt;Still not sure about power measurement...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Apr 2012 21:28:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TWR-MEM-MRAM-with-TWR-K53N512/m-p/157022#M455</guid>
      <dc:creator>J_Hunt</dc:creator>
      <dc:date>2012-04-27T21:28:53Z</dc:date>
    </item>
    <item>
      <title>Re: Using TWR-MEM MRAM with TWR-K53N512</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TWR-MEM-MRAM-with-TWR-K53N512/m-p/157023#M456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This problem have been solving by change line with number 20 in file "MK53N512CMD100.mem" from&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;usederivative "MK53N512CMD"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;to&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;usederivative "MK53DZ10"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Aug 2012 16:46:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-TWR-MEM-MRAM-with-TWR-K53N512/m-p/157023#M456</guid>
      <dc:creator>khabarov</dc:creator>
      <dc:date>2012-08-01T16:46:01Z</dc:date>
    </item>
  </channel>
</rss>