<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK60 ADC, Differential without PGA, VREFH vs VREF_OUT</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-ADC-Differential-without-PGA-VREFH-vs-VREF-OUT/m-p/746573#M45475</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #646464; background-color: #f2f2f5; font-size: 14px;"&gt;I am using the K60 16-bit ADC converters similar to what is described in AN-4568. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #646464; background-color: #f2f2f5; font-size: 14px;"&gt;I am using this in differential mode without PGA. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #646464; background-color: #f2f2f5; font-size: 14px;"&gt;When PGA is used it is clear that the VREF_OUT signal is required and the governing voltage reference for the measurement. However when PGA is not used [refer to Table 2, ADC16 MEASUREMENT (PGA DISABLED)] it not clear what effect VREF_OUT or VREFH play in the ADC conversion. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #646464; background-color: #f2f2f5; font-size: 14px;"&gt;Seemingly VREF_OUT is NOT needed in differential PGA disabled mode, yet the differential input range is limited to 2400mV. But where does this come from if VREF_OUT can be disabled? What effect, if any does VREFH input play in the measurement in this mode?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #646464; background-color: #f2f2f5; font-size: 14px;"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #646464; background-color: #f2f2f5; font-size: 14px;"&gt;PMT&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Nov 2017 17:26:46 GMT</pubDate>
    <dc:creator>pmt</dc:creator>
    <dc:date>2017-11-02T17:26:46Z</dc:date>
    <item>
      <title>K60 ADC, Differential without PGA, VREFH vs VREF_OUT</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-ADC-Differential-without-PGA-VREFH-vs-VREF-OUT/m-p/746573#M45475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #646464; background-color: #f2f2f5; font-size: 14px;"&gt;I am using the K60 16-bit ADC converters similar to what is described in AN-4568. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #646464; background-color: #f2f2f5; font-size: 14px;"&gt;I am using this in differential mode without PGA. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #646464; background-color: #f2f2f5; font-size: 14px;"&gt;When PGA is used it is clear that the VREF_OUT signal is required and the governing voltage reference for the measurement. However when PGA is not used [refer to Table 2, ADC16 MEASUREMENT (PGA DISABLED)] it not clear what effect VREF_OUT or VREFH play in the ADC conversion. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #646464; background-color: #f2f2f5; font-size: 14px;"&gt;Seemingly VREF_OUT is NOT needed in differential PGA disabled mode, yet the differential input range is limited to 2400mV. But where does this come from if VREF_OUT can be disabled? What effect, if any does VREFH input play in the measurement in this mode?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #646464; background-color: #f2f2f5; font-size: 14px;"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #646464; background-color: #f2f2f5; font-size: 14px;"&gt;PMT&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Nov 2017 17:26:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-ADC-Differential-without-PGA-VREFH-vs-VREF-OUT/m-p/746573#M45475</guid>
      <dc:creator>pmt</dc:creator>
      <dc:date>2017-11-02T17:26:46Z</dc:date>
    </item>
    <item>
      <title>Re: K60 ADC, Differential without PGA, VREFH vs VREF_OUT</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-ADC-Differential-without-PGA-VREFH-vs-VREF-OUT/m-p/746574#M45476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;Hi, Pmt&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The reference voltage of the PGA module is VREF_OUT, which is 1.2V. You can connect an external&amp;nbsp; 1.2V voltage source to VREF_OUT pin or configure the VREF module so that it can output 1.2V for VREF_OUT pin.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The reference voltage of&amp;nbsp; ADC16 module can be from VREF_OUT or VREFH pin, which is selected by the ADCx_SC2[REFSEL],if the &lt;/SPAN&gt;&lt;BR /&gt; &lt;SPAN style="font-size: 10.0pt;"&gt;ADCx_SC2[REFSEL]=00, the 3.3V voltage reference from(Vrefh,Vrefl) is selected. If &lt;/SPAN&gt;&lt;BR /&gt; &lt;SPAN style="font-size: 10.0pt;"&gt;ADCx_SC2[REFSEL]=01, the Vref_OUT 1.2V voltage reference is selected for ADC16 module.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;If you use PGA, generally, we suggest you use 1.2V Vref_OUT as voltage reference of ADC16, but you can still use 3.3V voltage reference from VREFH pin for ADC16 module.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;If you do not use PGA, in general, we suggest you use 3.3V voltage reference from VREFH pin, but you can still use VREF_OUT 1.2V as voltage reference of ADC16.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;If you use 3.3V voltage reference, the maximum ADC input voltage is 3.3V in single-ended mode, in differential mode, it is -3.3V~+3.3V, the Vpp is 6.6V. If you use 1.2V voltage reference, the maximum ADC input voltage is 1.2V in single-ended mode, in differential mode, it is -1.2V~+1.2V, the Vpp is 2.4V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;The AN4568 use 1.2V voltage reference for ADC16.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Hope it can help you&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Nov 2017 07:49:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-ADC-Differential-without-PGA-VREFH-vs-VREF-OUT/m-p/746574#M45476</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-11-03T07:49:49Z</dc:date>
    </item>
  </channel>
</rss>