<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMeasure current and voltage with K26</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Measure-current-and-voltage-with-K26/m-p/745393#M45387</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to measure current and voltage with MK26FN2M0VMI18&lt;/P&gt;&lt;P&gt;I have a DC input from 5V up to 28V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to measure it with a shunt resistor resistor of 0m50 and the ADC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If so, I need to use VREF or VREF_OUT ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://microcontrollerslab.com/wp-content/uploads/2015/05/Digital-Ammeter-using-pic-microcontroller.jpg"&gt;This circuit&lt;/A&gt; can serve ?, it is similar to my requirements. If so, I have to place the R1 closed to GND and R2 closed to K26F ADC pin?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jan 2018 13:03:56 GMT</pubDate>
    <dc:creator>javierhernande1</dc:creator>
    <dc:date>2018-01-22T13:03:56Z</dc:date>
    <item>
      <title>Measure current and voltage with K26</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Measure-current-and-voltage-with-K26/m-p/745393#M45387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to measure current and voltage with MK26FN2M0VMI18&lt;/P&gt;&lt;P&gt;I have a DC input from 5V up to 28V&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it possible to measure it with a shunt resistor resistor of 0m50 and the ADC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If so, I need to use VREF or VREF_OUT ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://microcontrollerslab.com/wp-content/uploads/2015/05/Digital-Ammeter-using-pic-microcontroller.jpg"&gt;This circuit&lt;/A&gt; can serve ?, it is similar to my requirements. If so, I have to place the R1 closed to GND and R2 closed to K26F ADC pin?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jan 2018 13:03:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Measure-current-and-voltage-with-K26/m-p/745393#M45387</guid>
      <dc:creator>javierhernande1</dc:creator>
      <dc:date>2018-01-22T13:03:56Z</dc:date>
    </item>
    <item>
      <title>Re: Measure current and voltage with K26</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Measure-current-and-voltage-with-K26/m-p/745394#M45388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Javier,&lt;/P&gt;&lt;P&gt;I guess this is a very low frequency ADC test circuit. The load and the battery will not change in a high frequency. So I think it is nessesary to put a small cap near the AD pad. Because in ADC there is a Cadin. It's value is around 5~10pf. You can see it in datasheet. Since there is a big resistor R2 before ADC, Cadin will cause AD value distort. I think the value of the CAP should over 50pf. Details please find in AN4373. You can search this document on NXP website. &lt;BR /&gt;As to VREF select, please refer to section 39.3.3(Voltage Reference Select) in reference manual. You can also use the examples in SDK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jan 2018 07:16:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Measure-current-and-voltage-with-K26/m-p/745394#M45388</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2018-01-23T07:16:30Z</dc:date>
    </item>
  </channel>
</rss>