<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Flash write for KE</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-write-for-KE/m-p/745097#M45373</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are right.&lt;/P&gt;&lt;P&gt;Now it is fine,,,&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Apr 2018 10:41:20 GMT</pubDate>
    <dc:creator>pietrodicastri</dc:creator>
    <dc:date>2018-04-19T10:41:20Z</dc:date>
    <item>
      <title>Flash write for KE</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-write-for-KE/m-p/745095#M45371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;I use the KE processor on the TWR-KE18F board, and I try to write in the flash. I used fluently the C90TFS driver for the K64, without any issues. Now I cannot erase, I get the error 0x20, Access violation.&lt;/P&gt;&lt;P&gt;I used the same settings as in the K64, it seems they are compatible in terms of the fields in the&amp;nbsp;FLASH_SSD_CONFIG structure, the difference is the ability of the FLEXNVM which I am not interested on.&lt;/P&gt;&lt;P&gt;But no way to have it working. I tested also the example and nothing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need a suggestion.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pietro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Apr 2018 13:43:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-write-for-KE/m-p/745095#M45371</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2018-04-18T13:43:25Z</dc:date>
    </item>
    <item>
      <title>Re: Flash write for KE</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-write-for-KE/m-p/745096#M45372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pietro&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using the KE18F in HSRUN mode because Flash operations can't be performed in this mode:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21319i309F14760ECF4C59/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;EM&gt;uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;SPAN&gt;Kinetis: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.utasker.com%2Fkinetis.html" rel="nofollow" target="_blank"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Apr 2018 14:53:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-write-for-KE/m-p/745096#M45372</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2018-04-18T14:53:21Z</dc:date>
    </item>
    <item>
      <title>Re: Flash write for KE</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-write-for-KE/m-p/745097#M45373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are right.&lt;/P&gt;&lt;P&gt;Now it is fine,,,&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Apr 2018 10:41:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Flash-write-for-KE/m-p/745097#M45373</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2018-04-19T10:41:20Z</dc:date>
    </item>
  </channel>
</rss>