<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKL82 Passive Pin Filter</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-Passive-Pin-Filter/m-p/744046#M45320</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question relating to Passive Pin Filter functionality for input GPIOs for a KL82 part.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the KL82 reference manual (attached), page 1598 there is table 53-1. For the &lt;EM&gt;Passive Filter Enable Enable Control&lt;/EM&gt;&amp;nbsp;line is says &lt;EM&gt;No&lt;/EM&gt; for all ports except PTA4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However in the KL82P121M72SF0 Datasheet&amp;nbsp; (attached) on page 40, for example the &lt;EM&gt;Passive pin Filter after POR&lt;/EM&gt; comes up as N (Disabled).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this mean that the Passive Pin Filter can be enabled for PTC6 for example? Which is the correct interpretation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Feb 2018 13:13:54 GMT</pubDate>
    <dc:creator>rtoma</dc:creator>
    <dc:date>2018-02-13T13:13:54Z</dc:date>
    <item>
      <title>KL82 Passive Pin Filter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-Passive-Pin-Filter/m-p/744046#M45320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question relating to Passive Pin Filter functionality for input GPIOs for a KL82 part.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the KL82 reference manual (attached), page 1598 there is table 53-1. For the &lt;EM&gt;Passive Filter Enable Enable Control&lt;/EM&gt;&amp;nbsp;line is says &lt;EM&gt;No&lt;/EM&gt; for all ports except PTA4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However in the KL82P121M72SF0 Datasheet&amp;nbsp; (attached) on page 40, for example the &lt;EM&gt;Passive pin Filter after POR&lt;/EM&gt; comes up as N (Disabled).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this mean that the Passive Pin Filter can be enabled for PTC6 for example? Which is the correct interpretation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Feb 2018 13:13:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-Passive-Pin-Filter/m-p/744046#M45320</guid>
      <dc:creator>rtoma</dc:creator>
      <dc:date>2018-02-13T13:13:54Z</dc:date>
    </item>
    <item>
      <title>Re: KL82 Passive Pin Filter</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-Passive-Pin-Filter/m-p/744047#M45321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Radu Toma&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to Reference manual:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Individual input passive filter field supporting enable and disable of the individual input passive filter on selected pins&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In both documents it is mentioned there is not passive filter control for&amp;nbsp;all ports except PTA4. N in datasheet is not for disable, it is for no available in the pin.&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Feb 2018 21:51:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL82-Passive-Pin-Filter/m-p/744047#M45321</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2018-02-20T21:51:30Z</dc:date>
    </item>
  </channel>
</rss>