<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックKinetisL Sample Code running on Codewarrior</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KinetisL-Sample-Code-running-on-Codewarrior/m-p/226340#M4527</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I've extracted sample codes from KL25_SC.exe, I'm refering to LQRUG_uart_ex1 example.&lt;/P&gt;&lt;P&gt;When I try to Import this project code warrior is giving error saying "No Projects are found to Import", next when I manually open this folder (Kinetis L Sample Code\kl25_sc\klxx-sc-baremetal\src\projects) there are only two files available LQRG_uart_ex1.c &amp;amp; isr.h. &lt;/P&gt;&lt;P&gt;Please help how to make this example work on code warrior, If I have to add any other dependencies how to add, please brief me on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can also see all these example projects provided in the barematel folder give the same problem, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mithun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Jan 2013 14:34:06 GMT</pubDate>
    <dc:creator>mithunp_s</dc:creator>
    <dc:date>2013-01-16T14:34:06Z</dc:date>
    <item>
      <title>KinetisL Sample Code running on Codewarrior</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KinetisL-Sample-Code-running-on-Codewarrior/m-p/226340#M4527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;I've extracted sample codes from KL25_SC.exe, I'm refering to LQRUG_uart_ex1 example.&lt;/P&gt;&lt;P&gt;When I try to Import this project code warrior is giving error saying "No Projects are found to Import", next when I manually open this folder (Kinetis L Sample Code\kl25_sc\klxx-sc-baremetal\src\projects) there are only two files available LQRG_uart_ex1.c &amp;amp; isr.h. &lt;/P&gt;&lt;P&gt;Please help how to make this example work on code warrior, If I have to add any other dependencies how to add, please brief me on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can also see all these example projects provided in the barematel folder give the same problem, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mithun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2013 14:34:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KinetisL-Sample-Code-running-on-Codewarrior/m-p/226340#M4527</guid>
      <dc:creator>mithunp_s</dc:creator>
      <dc:date>2013-01-16T14:34:06Z</dc:date>
    </item>
    <item>
      <title>Re: KinetisL Sample Code running on Codewarrior</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KinetisL-Sample-Code-running-on-Codewarrior/m-p/226341#M4528</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem there is the projects you can't open are only available for IAR and KEIL, we have plans to migrate many of them to CodeWarrior but we haven't defined a specific date to do so.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry about this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2013 20:23:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KinetisL-Sample-Code-running-on-Codewarrior/m-p/226341#M4528</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2013-01-16T20:23:21Z</dc:date>
    </item>
  </channel>
</rss>