<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: MK22DX256VMC5 VOUT33 output not good when VREGIN changes</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741458#M45195</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiangjun,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But we will &lt;STRONG&gt;use the USB&lt;/STRONG&gt; function, and if we &lt;STRONG&gt;use the external LDO&lt;/STRONG&gt;, how to treat with &lt;STRONG&gt;VREGIN and VOUT3.3&lt;/STRONG&gt;?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Dec 2017 00:22:17 GMT</pubDate>
    <dc:creator>huijiejiang</dc:creator>
    <dc:date>2017-12-06T00:22:17Z</dc:date>
    <item>
      <title>MK22DX256VMC5 VOUT33 output not good when VREGIN changes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741453#M45190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using the internal regulator, and VOUT33 output voltage(+3.3V on the schematic) rise to 3.8V when there is an fast voltage dip on VREGIN("+5V" on the sch, "+5Vout" in the graph), see below for the sch and&amp;nbsp;graph.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We guess that is because of the PSRR, but we cannot find the PSRR parameter in the datasheet...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the root cause and how can we improve the performance?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="connection.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/37926iA89330E19BE21BDF/image-size/large?v=v2&amp;amp;px=999" role="button" title="connection.PNG" alt="connection.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="tek00001.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38001i3E0CC90C9FCFD309/image-size/large?v=v2&amp;amp;px=999" role="button" title="tek00001.png" alt="tek00001.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="tek00002.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38104i1F439441F603D57E/image-size/large?v=v2&amp;amp;px=999" role="button" title="tek00002.png" alt="tek00002.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Nov 2017 00:49:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741453#M45190</guid>
      <dc:creator>huijiejiang</dc:creator>
      <dc:date>2017-11-28T00:49:57Z</dc:date>
    </item>
    <item>
      <title>Re: MK22DX256VMC5 VOUT33 output not good when VREGIN changes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741454#M45191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, HuJie,&lt;/P&gt;&lt;P&gt;The VDD power supply ranges from -0.3V to 3.8V, so I think it is okay.&lt;/P&gt;&lt;P&gt;As you know that the VOUT33 is&amp;nbsp; the internal regulator output, the internal regulator inputs 5V, it is not related to the PSRR(power supply rejection rate). how about&amp;nbsp; using different capacitor on the VOUT33 pin, which can ranges from 1.76uF to 8.16uF.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Nov 2017 07:55:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741454#M45191</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-11-28T07:55:37Z</dc:date>
    </item>
    <item>
      <title>Re: MK22DX256VMC5 VOUT33 output not good when VREGIN changes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741455#M45192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiangjun,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your quickly reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried your suggestion to add additional capacitors to C9 and made it as 4.4uf, 6.6uf..., and did the test with the same method, but there was no improvement.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Based on the test, the fluctuation of the VOUT3.3 is reduced when the voltage dip is reduced and seams not so related to the capacitor, which meets the requirement of the datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the question,&lt;/P&gt;&lt;P&gt;1) Do you have the PSRR of&amp;nbsp;the&amp;nbsp;regulator?&lt;/P&gt;&lt;P&gt;2) Is there any additional requirement for the&amp;nbsp;VREGIN that related with VOUT3.3?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Nov 2017 05:08:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741455#M45192</guid>
      <dc:creator>huijiejiang</dc:creator>
      <dc:date>2017-11-29T05:08:39Z</dc:date>
    </item>
    <item>
      <title>Re: MK22DX256VMC5 VOUT33 output not good when VREGIN changes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741456#M45193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiangjun,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any update?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regarding the internal regulator,&lt;/P&gt;&lt;P&gt;We design the MCU as a USB device, if we use an external LDO, how to treat the VREGIN and VOUT3.3?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do we&amp;nbsp;MUST to, as the below picture,&lt;/P&gt;&lt;P&gt;1) connect VREGIN to VBUS&lt;/P&gt;&lt;P&gt;2) add Cstab to VOUT3.3(2.2uf? can that capacitor be used a smaller value one?)&lt;/P&gt;&lt;P&gt;3) connect VDD to external LDO output&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Untitled.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52362i9F943B9F4C8EE8D7/image-size/large?v=v2&amp;amp;px=999" role="button" title="Untitled.png" alt="Untitled.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;EM&gt;&lt;STRONG&gt;Can we ONLY use the external LDO and just leave away(just float the VREGIN and VOUT3.3) the internal regulator?&lt;/STRONG&gt;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Dec 2017 10:12:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741456#M45193</guid>
      <dc:creator>huijiejiang</dc:creator>
      <dc:date>2017-12-01T10:12:05Z</dc:date>
    </item>
    <item>
      <title>Re: MK22DX256VMC5 VOUT33 output not good when VREGIN changes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741457#M45194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;SPAN class=""&gt;HuiJie,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;If you use external LDO to provide power for the K22,&amp;nbsp; internal regulator is NOT used, in the case, when USB is not used in the application, it is recommended to&lt;BR /&gt;connect VREGOUT and VREG_INx together and tie to ground&lt;BR /&gt;through a 10kΩ resistor. Do not tie directly to ground, as this&lt;BR /&gt;causes a latch-up risk. For systems where only one of the&lt;BR /&gt;VREG_INx pins is ever used, it is also recommended to&lt;BR /&gt;connect the two VREG_INx pins together.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;BR&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Xiangjun rong&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Dec 2017 05:54:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741457#M45194</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-12-05T05:54:08Z</dc:date>
    </item>
    <item>
      <title>Re: MK22DX256VMC5 VOUT33 output not good when VREGIN changes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741458#M45195</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xiangjun,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But we will &lt;STRONG&gt;use the USB&lt;/STRONG&gt; function, and if we &lt;STRONG&gt;use the external LDO&lt;/STRONG&gt;, how to treat with &lt;STRONG&gt;VREGIN and VOUT3.3&lt;/STRONG&gt;?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Dec 2017 00:22:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741458#M45195</guid>
      <dc:creator>huijiejiang</dc:creator>
      <dc:date>2017-12-06T00:22:17Z</dc:date>
    </item>
    <item>
      <title>Re: MK22DX256VMC5 VOUT33 output not good when VREGIN changes</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741459#M45196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;If you use USB, you have to use internal regulator to provide power for internal USB transceiver. In the case, you can connect VREGIN to 5V, connect the VOUT33 pin to a 2.2uF capacitor, connect the VDD pins to external 3.3V power supply, you can get 3.3V power supply with an external LDO or general regulator such as LM1117-3.3V device.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;'XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Dec 2017 06:07:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK22DX256VMC5-VOUT33-output-not-good-when-VREGIN-changes/m-p/741459#M45196</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-12-06T06:07:39Z</dc:date>
    </item>
  </channel>
</rss>