<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: How do I run a servo motor using a tmp35 sensor on a KL43z freedom board ?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-run-a-servo-motor-using-a-tmp35-sensor-on-a-KL43z/m-p/740269#M45118</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Mohammed,&lt;/P&gt;&lt;P&gt;You can calculate the TMP35 output voltage at the room temperature, then calculate the ADC sample value at the output voltage as a threshold based on ADC bitwidth. In the application code, use PIT to generate ISR, in the ISR, start ADC sampling, if the sample is greater than the threshold, start the motor.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Mar 2018 08:12:54 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2018-03-29T08:12:54Z</dc:date>
    <item>
      <title>How do I run a servo motor using a tmp35 sensor on a KL43z freedom board ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-run-a-servo-motor-using-a-tmp35-sensor-on-a-KL43z/m-p/740266#M45115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm doing a project on the freedom board kl43z but there isn't&amp;nbsp;much material online for help. I'm&amp;nbsp;confused how to code to read the temperature as the input using a tmp35 sensor which causes the servo motor to start moving at a certain temp( room temperature).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Mar 2018 14:33:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-run-a-servo-motor-using-a-tmp35-sensor-on-a-KL43z/m-p/740266#M45115</guid>
      <dc:creator>mohammedsiddiq</dc:creator>
      <dc:date>2018-03-27T14:33:12Z</dc:date>
    </item>
    <item>
      <title>Re: How do I run a servo motor using a tmp35 sensor on a KL43z freedom board ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-run-a-servo-motor-using-a-tmp35-sensor-on-a-KL43z/m-p/740267#M45116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Mohammed,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The KL43Z has on-chip 16 bits ADC and 1.2V voltage reference, the ADC can sample the TMP35 output voltage. What is the temperature range for your application?&lt;/P&gt;&lt;P&gt;I have checked the data sheet of TMP35, at 25 C, it outputs 250mV, the output scale factor is 10mV/C. As you know that the ADC has Voltage reference pin Vrefsh which can be connected to internal 1.2V voltage reference, in the case, you can connect the TMP35 output to ADC analog pin directly with OP AMP you can connect a serial 100 ohm resistor and 2.2nF capacitor(between analog GND and ADC analog pin) as a simple filter, it is okay.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Mar 2018 03:36:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-run-a-servo-motor-using-a-tmp35-sensor-on-a-KL43z/m-p/740267#M45116</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-03-28T03:36:34Z</dc:date>
    </item>
    <item>
      <title>Re: How do I run a servo motor using a tmp35 sensor on a KL43z freedom board ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-run-a-servo-motor-using-a-tmp35-sensor-on-a-KL43z/m-p/740268#M45117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I figured that out but im&amp;nbsp;having trouble how to code not sure how would i go about to code it basically&amp;nbsp;&lt;BR /&gt;I wrote some code and its reading the temperature or at least I think it is but not sure how to move the motor according to room temperature ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Mar 2018 03:41:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-run-a-servo-motor-using-a-tmp35-sensor-on-a-KL43z/m-p/740268#M45117</guid>
      <dc:creator>mohammedsiddiq</dc:creator>
      <dc:date>2018-03-28T03:41:23Z</dc:date>
    </item>
    <item>
      <title>Re: How do I run a servo motor using a tmp35 sensor on a KL43z freedom board ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-run-a-servo-motor-using-a-tmp35-sensor-on-a-KL43z/m-p/740269#M45118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Mohammed,&lt;/P&gt;&lt;P&gt;You can calculate the TMP35 output voltage at the room temperature, then calculate the ADC sample value at the output voltage as a threshold based on ADC bitwidth. In the application code, use PIT to generate ISR, in the ISR, start ADC sampling, if the sample is greater than the threshold, start the motor.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Mar 2018 08:12:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-do-I-run-a-servo-motor-using-a-tmp35-sensor-on-a-KL43z/m-p/740269#M45118</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-03-29T08:12:54Z</dc:date>
    </item>
  </channel>
</rss>