<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: common mode range</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/common-mode-range/m-p/735861#M44930</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is still a bit ambiguous as there is also a pin on the package labeled VREFH which I have tied to 3v3 but I am using internal 1.2v reference so is max VADIN 31/32 of 1.2v (selected VREF) or 31/32 of 3.3V (package pin).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jun 2018 03:40:00 GMT</pubDate>
    <dc:creator>jakebailey</dc:creator>
    <dc:date>2018-06-06T03:40:00Z</dc:date>
    <item>
      <title>common mode range</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/common-mode-range/m-p/735859#M44928</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the common mode input range of K22 differential ADC? I assumed it would be reasonably close to the supply rails but this does not appear to be the case as inputting common mode signals above&amp;nbsp;1.2 vref starts to cause distortion.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 May 2018 17:01:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/common-mode-range/m-p/735859#M44928</guid>
      <dc:creator>jakebailey</dc:creator>
      <dc:date>2018-05-30T17:01:20Z</dc:date>
    </item>
    <item>
      <title>Re: common mode range</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/common-mode-range/m-p/735860#M44929</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can find the VADIN in DataSheet.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="VADIN.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17464i9D0D770D265ECCAE/image-size/large?v=v2&amp;amp;px=999" role="button" title="VADIN.png" alt="VADIN.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 01:47:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/common-mode-range/m-p/735860#M44929</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2018-06-06T01:47:47Z</dc:date>
    </item>
    <item>
      <title>Re: common mode range</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/common-mode-range/m-p/735861#M44930</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is still a bit ambiguous as there is also a pin on the package labeled VREFH which I have tied to 3v3 but I am using internal 1.2v reference so is max VADIN 31/32 of 1.2v (selected VREF) or 31/32 of 3.3V (package pin).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jun 2018 03:40:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/common-mode-range/m-p/735861#M44930</guid>
      <dc:creator>jakebailey</dc:creator>
      <dc:date>2018-06-06T03:40:00Z</dc:date>
    </item>
    <item>
      <title>Re: common mode range</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/common-mode-range/m-p/735862#M44931</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ADC Reference Options.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/31750i0FDFB7269CDC69F7/image-size/large?v=v2&amp;amp;px=999" role="button" title="ADC Reference Options.png" alt="ADC Reference Options.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;ADCx_SC2[REFSEL] bit selects the voltage reference sources for ADC.&lt;BR /&gt;When 1.2 V VREF_OUT is selected, the The max VADIN is 31/32 of 1.2v. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Robin&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jun 2018 08:04:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/common-mode-range/m-p/735862#M44931</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2018-06-07T08:04:32Z</dc:date>
    </item>
  </channel>
</rss>