<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K65 RUNHS mode memset performance is worst than RUN mode.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-RUNHS-mode-memset-performance-is-worst-than-RUN-mode/m-p/734198#M44873</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I find the same question at online support system with case number: 00151005&lt;/P&gt;&lt;P&gt;Please check my feedback at case number: 00151005.&lt;/P&gt;&lt;P&gt;Thank you for the understanding.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 11 Feb 2018 05:32:33 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2018-02-11T05:32:33Z</dc:date>
    <item>
      <title>K65 RUNHS mode memset performance is worst than RUN mode.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-RUNHS-mode-memset-performance-is-worst-than-RUN-mode/m-p/734197#M44872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am doing some bench-marking on the K65 processor and have seen a strange problem. When the core is run in RUNHS mode (Core = 180MHz, SDRAM = 60MHz, Flash = 25.7MHz), I get ~34MBps performance for memset operation. However, with RUN mode (Core = 120MHz, SDRAM = 60MHz, Flash = 20MHz), I get ~52MBps performance for memset operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My code is running is from the Flash and I use external SDRAM for data. Can any body help me understand this strange behavior?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Feb 2018 11:31:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-RUNHS-mode-memset-performance-is-worst-than-RUN-mode/m-p/734197#M44872</guid>
      <dc:creator>irfanshahid</dc:creator>
      <dc:date>2018-02-09T11:31:47Z</dc:date>
    </item>
    <item>
      <title>Re: K65 RUNHS mode memset performance is worst than RUN mode.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-RUNHS-mode-memset-performance-is-worst-than-RUN-mode/m-p/734198#M44873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I find the same question at online support system with case number: 00151005&lt;/P&gt;&lt;P&gt;Please check my feedback at case number: 00151005.&lt;/P&gt;&lt;P&gt;Thank you for the understanding.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Mike&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Feb 2018 05:32:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-RUNHS-mode-memset-performance-is-worst-than-RUN-mode/m-p/734198#M44873</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2018-02-11T05:32:33Z</dc:date>
    </item>
  </channel>
</rss>