<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックAdding two FRDM- KL25Z Microcontroller</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Adding-two-FRDM-KL25Z-Microcontroller/m-p/733911#M44862</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the best way to use two microcontrollers&amp;nbsp;in autonomous car with out any conflict in the orders? The first microcontroller will be used for the speed process, and the other one will be used for the two line cameras?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Jan 2018 22:31:03 GMT</pubDate>
    <dc:creator>khalidal-dawoud</dc:creator>
    <dc:date>2018-01-17T22:31:03Z</dc:date>
    <item>
      <title>Adding two FRDM- KL25Z Microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Adding-two-FRDM-KL25Z-Microcontroller/m-p/733911#M44862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the best way to use two microcontrollers&amp;nbsp;in autonomous car with out any conflict in the orders? The first microcontroller will be used for the speed process, and the other one will be used for the two line cameras?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 22:31:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Adding-two-FRDM-KL25Z-Microcontroller/m-p/733911#M44862</guid>
      <dc:creator>khalidal-dawoud</dc:creator>
      <dc:date>2018-01-17T22:31:03Z</dc:date>
    </item>
    <item>
      <title>Re: Adding two FRDM- KL25Z Microcontroller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Adding-two-FRDM-KL25Z-Microcontroller/m-p/733912#M44863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The KL25 UART module supports LIN bus, which could be used as a LIN slave in CAR network.&lt;/P&gt;&lt;P&gt;NXP provides the &lt;A href="https://www.nxp.com/downloads/en/device-drivers/FSL_LIN_2.X_STACK.zip"&gt;LIN2.x and SAE J2602 Stack(REV v4.5.9)&lt;/A&gt;, which supports KEA product so far.&lt;/P&gt;&lt;P&gt;If customer consider the communication speed, customer could select a MCU with CAN module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;best regards,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jan 2018 03:20:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Adding-two-FRDM-KL25Z-Microcontroller/m-p/733912#M44863</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2018-01-19T03:20:02Z</dc:date>
    </item>
  </channel>
</rss>